Stream Settings
stream.auto_close
Abbreviation
st a
Access
get/set
Description
This setting is intended for all network related streams:
- tcp/udp clients
- tcp server clients
- http_get/http_post
When
false
, a stream handle is not reused until it is manually closed. In this case, the
stream_poll
command returns
2
(remote closed connection) for a stream when the associated client has disconnected. See
stream_poll
.
When
true
, a stream handle is automatically reused when closed.
Note: When
stream.auto_close
is
true
, TCP/HTTP/WebSocket client/server streams remain open until all RX data has been read. Even if the remote side has closed the connection, the stream remains open until all RX data has been read. In this case, polling the stream returns
2
.
Arguments
<1|true|on/0|false|off>
where
-
0orfalseoroff: auto close disabled -
1ortrueoron: auto close enabled
Default
true
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get st a
1
>
Set example
> set st a false
Set OK