Network
network.arp.lock_enabled
Abbreviation
ne a l
Access
get/set
Description
Lock destination ARP entry to avoid streaming delays due to address resolution.
Before an IP packet can be transmitted/received the network stack needs to resolve the IP address into a MAC address. This is done with Address Resolution Protocol (ARP).
When the IP is resolved it is cached in the ARP table. Due to RAM limitations, the ARP table can store only a limited number of entries. Old entries are replaced by new ones.
This can cause intermittent delays when streaming data via TCP/UDP. During TCP/UDP transmission, if the socket's destination MAC is replaced in the ARP cache, ARP needs to resolve the destination MAC address before the next TCP/UDP packet can go out. ARP can take 100s of ms.
To avoid these intermittent delays, you can lock the destination ARP entry when streaming by setting
network.arp.lock_enabled
to true.
If
network.arp.lock_enabled
is true, after a TCP client/server, UDP client/server, or websocket client/server stream is opened, the remote side's ARP entry is stored in a static part of the ARP cache.
When the stream is closed, the static entry is removed.
The socket then streams without ARPs.
Note : It is recommended to increase the value of network.arp.table_size when using this feature.
Arguments
<1|true|on/0|false|off>
Default
0
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Set example
> set ne a l true
R000008
Set OK
Get example
> get ne a l
R000003
0
network.arp.table_size
Abbreviation
ne a t
Access
get/set
Description
Configures the maximum number of entries to cache in the ARP table. See network.arp.lock_enabled .
Arguments
<max_entries>
where
<max_entries>
is an integer from
3
to
16
.
Default
8
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Set example
> set ne a t 5
R000008
Set OK
Get example
> get ne a t
R000003
3
network.buffer.rxtx_ratio
Abbreviation
ne b r
Access
get/set
Description
The percentage of the network buffer allocated to Rx.
Rx buffer pool size = network.buffer.size x (network.buffer.rxtx_ratio / 100)
Tx buffer pool size = network.buffer.size x ((100 - network.buffer.rxtx_ratio) / 100)
Value limits (%): Min: 10 Max: 90
Arguments
<percent_rx>
Default
50
Properties
Gecko OS Kernel Plugin
Set example
> set ne b r 20
R000008
Set OK
Get example
> get ne b r
R000004
20
network.buffer.control_size
Abbreviation
ne b c
Access
get/set
Description
Configure the size of the network buffer used for control packets. This buffer is typically used for I/O control packets to the Wi-Fi chip, TCP fragment buffers, and TCP ACK/NAK packets. If data writes are sufficiently large (of the order of hundreds of bytes), 4K (the default
4096
bytes) is sufficient for the control buffer.
The control buffer may become depleted if data writes are small (of the order of several bytes).
Note : network.buffer.rxtx_ratio has no effect on this buffer.
Arguments
<bytes>
where
<bytes>
is in the range
2048
to
32768
Default
8192
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Set example
> set ne b c 22528
R000008
Set OK
Get example
> get ne b c
R000006
4096
network.buffer.size
Abbreviation
ne b s
Access
get/set
Description
The total size of the network buffers, in bytes.
his is important for applications that have asymmetric data throughput requirements. If your app is heavily Tx (or Rx) centric, you can adjust the Tx and Rx buffer sizes accordingly to achieve maximum throughput.
This buffer is divided between the rx/tx buffers based on the network.buffer.rxtx_ratio variable.
This value is the amount of memory allocated from the dynamic memory section. The larger this value, the less memory available for other features.
This is an advanced feature. Take care when adjusting this value. The system may become unstable with certain values in certain applications.
Value limits and defaults (KB = 1024 bytes):
| Module | Min (bytes) | Min (KB) | Max (bytes) | Max (KB) | Default (bytes) | Default (KB) |
|---|---|---|---|---|---|---|
| WGM160P |
10000
|
9.8KB |
70000
|
68.3KB |
61440
|
60KB |
Arguments
<bytes>
where:
-
<bytes>is in the range10000to70000
Default
61440
(60KB)
Properties
Gecko OS Kernel Plugin
Set example
> set ne b s 22528
R000008
Set OK
Get example
> get ne b s
R000007
22528
network.buffer.usage
Abbreviation
ne b u
Access
get
Description
The approximate usage of the network TX & RX buffers as an integer percentage.
Arguments
-
Default
-
Gecko OS Kernel Plugin
Get example
> get ne b u
R000013
RX:13,TX:78
network.default_interface
Abbreviation
ne f
Access
get/set
Description
The default network interface used by various network commands and variables.
Commands:
Variables:
Arguments
<wlan/softap>
Default
wlan
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get ne f
R000006
wlan
Set example
> set ne f softap
R000008
Set OK
network.dns.timeout
Abbreviation
ne d t
Access
get
Description
This variable controls the amount of time the device will wait while it attempts to resolve a hostname via DNS.
Note : This timeout is applied to all hostname resolutions, i.e. it is applied to TCP/UDP/HTTP and so on.
See Networking and Security, DNS Client .
Arguments
<timeout ms>
where:
-
<timeout ms>is the amount of time to wait, in ms. Valid range is 100 to 10000.
Default
6000
Gecko OS Kernel Plugin
Get example
> get ne d t
R000006
6000
Set example
> set ne d t 8000
R000008
Set OK
network.tcp.delivery_type
Abbreviation
ne c d
Access
get/set
Description
Choose optimization strategy for TCP timers.
This variable configures the internal TCP timers for the required application.
In applications other than real-time streaming applications, the strategy is set to
normal
, to balance reliability, low latency, and throughput. For example, for cloud/internet applications the
normal
delivery type optimization is appropriate.
For real-time streaming applications, it may be preferable to optimize for low latency, with some sacrifice in reliability. For example, streaming TCP data via a softAP connection may require the
realtime
delivery type optimization.
Note : This configures the delivery type for all TCP connections that are opened after this value is set.
Arguments
<normal / realtime>
where:
-
normal- recommended setting for most applications. It has the best tradeoff between reliability, low latency, and throughput -
realtime- recommended for real-time streaming applications.
Default
normal
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get ne c d
R000008
normal
Set example
> set ne c d realtime
R000008
Set OK
network.tls.ca_cert
Abbreviation
ne t a
Access
get/set
Description
The default CA TLS certificate used with TLS network streams.
Note
: PEM file format requires Unix format line termination: LF (\n), not Windows format: CR-LF (\r\n). Some terminal applications may append unwanted end-of-line characters. Incorrect line termination may result in TLS connection failure.
Arguments
<CA TLS cert filename>
Default
globalsign_ca.pem
Properties
- takes effect immediately
- available in Safe Mode
Gecko OS Kernel Plugin
Get example
> get ne t a
R000017
geotrust_ca.pem
Set example
> set ne t a globalsign_ca.pem
R000008
Set OK
network.tls.ca_cert_verify_enabled
Abbreviation
ne t e
Access
get/set
Description
This variable allows optional disabling of TLS server certificate verification. By default verification is required.
When
network.tls.ca_verify_enabled
is true, if the server certificate is invalid, TLS connection is aborted.
When
network.tls.ca_verify_enabled
is false, if the server certificate is invalid, TLS connection continues with a warning.
Arguments
0|off|false/1|on|true
Default
1
Properties
- takes effect immediately
- available in Safe Mode
Gecko OS Kernel Plugin
Get example
> get ne t e
R000017
1
Set example
> set ne t a 0
R000003
Set OK
network.tls.client_cert
Abbreviation
ne t c
Access
get/set
Description
The filename of the TLS client cert.
Arguments
<TLS cert filename>
Default
null
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get ne t c
Set example
> set ne t c client_cert.pem
R000008
Set OK
network.tls.client_key
Abbreviation
ne t k
Access
get/set
Description
The filename of the TLS client cert key.
Arguments
<TLS cert key filename>
Default
null
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get ne t k
Set example
> set ne t k client_cert_key_filename
R000008
Set OK
network.tls.handshake_timeout
Abbreviation
ne t h
Access
get/set
Description
This specifies the maximum amount of time in seconds between handshake packets to wait before aborting the connection.
Arguments
<seconds>
where:
-
: Range: 3-600
Default
15
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get ne t h
15
Set example
> set ne t v 20
R000008
Set OK
network.tls.version
Abbreviation
ne t v
Access
get/set
Description
Specifies the maximum TLS version used. By default the client/server negotiates which TLS version/cipher to use but sometimes it is necessary to force a maximum version.
Arguments
<10/12>
where:
-
10: indicates TLS1.0 -
12: indicates TLS1.2
Default
12
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get ne t v
12
Set example
> set ne t v 10
R000008
Set OK