PCNT_Init_TypeDef Struct Reference
Initialization structure.
#include <em_pcnt.h>
Data Fields | |
PCNT_Mode_TypeDef | mode |
Mode to operate in. | |
uint32_t | counter |
Initial counter value (refer to reference manual for max value allowed). | |
uint32_t | top |
Initial top value (refer to reference manual for max value allowed). | |
bool | negEdge |
Polarity of incoming edge. | |
bool | countDown |
Counting direction, only applicable for pcntModeOvsSingle and pcntModeExtSingle modes. | |
bool | filter |
Enable filter, only available in pcntModeOvsSingle* mode. | |
bool | hyst |
Set to true to enable hysteresis. | |
bool | s1CntDir |
Set to true to enable S1 to determine the direction of counting in OVSSINGLE or EXTCLKSINGLE modes. | |
PCNT_CntEvent_TypeDef | cntEvent |
Selects whether the regular counter responds to up-count events, down-count events, both, or none. | |
PCNT_CntEvent_TypeDef | auxCntEvent |
Selects whether the auxiliary counter responds to up-count events, down-count events, both, or none. | |
PCNT_PRSSel_TypeDef | s0PRS |
Select PRS channel as input to S0IN in PCNTx_INPUT register. | |
PCNT_PRSSel_TypeDef | s1PRS |
Select PRS channel as input to S1IN in PCNTx_INPUT register. | |
Initialization structure.
Field Documentation
◆ mode
PCNT_Mode_TypeDef PCNT_Init_TypeDef::mode |
Mode to operate in.
◆ counter
uint32_t PCNT_Init_TypeDef::counter |
Initial counter value (refer to reference manual for max value allowed).
Only used for pcntModeOvsSingle (and possibly pcntModeDisable) modes. If using pcntModeExtSingle or pcntModeExtQuad modes, counter value is reset to HW reset value.
◆ top
uint32_t PCNT_Init_TypeDef::top |
Initial top value (refer to reference manual for max value allowed).
Only used for pcntModeOvsSingle (and possibly pcntModeDisable) modes. If using pcntModeExtSingle or pcntModeExtQuad modes, top value is reset to HW reset value.
◆ negEdge
bool PCNT_Init_TypeDef::negEdge |
Polarity of incoming edge.
- pcntModeExtSingle mode - if false, positive edges are counted, otherwise negative edges.
- pcntModeExtQuad mode - if true, counting direction is inverted.
◆ countDown
bool PCNT_Init_TypeDef::countDown |
Counting direction, only applicable for pcntModeOvsSingle and pcntModeExtSingle modes.
◆ filter
bool PCNT_Init_TypeDef::filter |
Enable filter, only available in pcntModeOvsSingle* mode.
◆ hyst
bool PCNT_Init_TypeDef::hyst |
Set to true to enable hysteresis.
When enabled, PCNT will always overflow and underflow to TOP/2.
◆ s1CntDir
bool PCNT_Init_TypeDef::s1CntDir |
Set to true to enable S1 to determine the direction of counting in OVSSINGLE or EXTCLKSINGLE modes.
When S1 is high, the count direction is given by CNTDIR, and when S1 is low, the count direction is the opposite.
◆ cntEvent
PCNT_CntEvent_TypeDef PCNT_Init_TypeDef::cntEvent |
Selects whether the regular counter responds to up-count events, down-count events, both, or none.
◆ auxCntEvent
PCNT_CntEvent_TypeDef PCNT_Init_TypeDef::auxCntEvent |
Selects whether the auxiliary counter responds to up-count events, down-count events, both, or none.
◆ s0PRS
PCNT_PRSSel_TypeDef PCNT_Init_TypeDef::s0PRS |
Select PRS channel as input to S0IN in PCNTx_INPUT register.
◆ s1PRS
PCNT_PRSSel_TypeDef PCNT_Init_TypeDef::s1PRS |
Select PRS channel as input to S1IN in PCNTx_INPUT register.