em_usbxpress_internal.h File Reference

Primary header file. Contains internal global declarations and definitions.

Version
5.4.0

License

Copyright 2016 Silicon Laboratories, Inc. http://www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file em_usbxpress_internal.h .

#include <stdint.h>
#include <stdbool.h>
#include " em_usb.h "

Macros

#define APIEA_GIE 0x01
#define APIEA_GIE_TEMP 0x02
#define SI_CP210X_GET_PART_NUMBER 0x370B
Value.
#define SI_CP210X_REQUEST 0xFF
Request.
#define SI_USBXPRESS_CLEAR_TO_SEND 0x0002
Value.
#define SI_USBXPRESS_FLUSH_BUFFERS 0x0001
Value.
#define SI_USBXPRESS_GET_VERSION 0x0008
Value.
#define SI_USBXPRESS_NOT_CLEAR_TO_SEND 0x0004
Value.
#define SI_USBXPRESS_PART_NUMBER_EFM32 0x81
EFM32 USBXpress Part Number.
#define SI_USBXPRESS_PART_NUMBER_EFM8 0x80
EFM8 USBXpress Part Number.
#define SI_USBXPRESS_REQUEST 0x02
Request.
#define USBXCORE_MAXLEN 19
#define USBXPRESS_LIBRARY_VERSION 0x0500

Functions

void USBX_DeviceStateChangeCb ( USBD_State_TypeDef oldState, USBD_State_TypeDef newState)
USB device state change call-back.
int USBX_inXferCompleteCb ( USB_Status_TypeDef , uint16_t, uint16_t remaining)
USBXpress IN Endpoint Transfer Complete Callback.
void USBX_jumpCallback (void)
Conditionally jumps to the user call-back routine.
int USBX_outXferCompleteCb ( USB_Status_TypeDef , uint16_t, uint16_t remaining)
USBXpress OUT Endpoint Transfer Complete Callback.
void USBX_ResetCb (void)
USB Reset call-back.
int USBX_SetupCmdCb (const USB_Setup_TypeDef *setup)
USB setup command call-back.
void USBXCORE_Read (uint8_t *, uint8_t *, uint8_t)
void USBXCORE_resetState (void)
Resets internal USBXpress variables.
void USBXCORE_Write (uint8_t *, uint8_t *, uint8_t)

Variables

uint32_t USBXCORE_apiEa
Enable or disable status of USB_API interrupts.
uint32_t USBXCORE_apiIntValue
Byte holding the current USB_API interrupts.
uint32_t * USBXCORE_byteCountInPtr
Pointer to variable holding number of bytes written.
uint32_t * USBXCORE_byteCountOutPtr
Pointer to variable holding number of bytes read.
uint8_t USBXCORE_configDesc [32]
Copy of configuration descriptor.
uint32_t USBXCORE_readSize
Number of bytes sent to USBX_blockRead() as numBytes.
uint32_t USBXCORE_writeSize
Number of bytes sent to USBX_blockWrite() as numBytes.

Macro Definition Documentation

#define APIEA_GIE   0x01
#define APIEA_GIE_TEMP   0x02

Temporary storage of API GIE bit when internally disabled

Definition at line 41 of file em_usbxpress_internal.h .

Referenced by USBX_SetupCmdCb() .

#define USBXCORE_MAXLEN   19

Maximum length of array passed by USBXCORE_Read/Write

Definition at line 47 of file em_usbxpress_internal.h .

#define USBXPRESS_LIBRARY_VERSION   0x0500

USBXpress firmware library version Example: 0x0241 => v2.41

Definition at line 31 of file em_usbxpress_internal.h .

Referenced by USBX_getLibraryVersion() .

Function Documentation

void USBX_DeviceStateChangeCb ( USBD_State_TypeDef oldState,
USBD_State_TypeDef newState
)

USB device state change call-back.

Set new state and jump to user API call-back.

Definition at line 71 of file em_usbxpress_callback.c .

References APIEA_GIE , USBD_STATE_CONFIGURED , USBD_STATE_SUSPENDED , USBX_DEV_CONFIGURED , USBX_DEV_SUSPEND , USBX_jumpCallback() , USBXCORE_apiEa , USBXCORE_apiIntValue , and USBXCORE_resetState() .

Referenced by USBX_init() .

int USBX_inXferCompleteCb ( USB_Status_TypeDef status,
uint16_t xferred,
uint16_t remaining
)

USBXpress IN Endpoint Transfer Complete Callback.

Gets the number of IN bytes transferred and passes them to the user API call-back.

Definition at line 242 of file em_usbxpress_callback.c .

References APIEA_GIE , USB_FS_BULK_EP_MAXSIZE , USB_STATUS_OK , USBD_Write() , USBX_jumpCallback() , USBX_TX_COMPLETE , USBXCORE_apiEa , USBXCORE_apiIntValue , USBXCORE_byteCountInPtr , and USBXCORE_writeSize .

Referenced by USBX_blockWrite() .

void USBX_jumpCallback ( void )

Conditionally jumps to the user call-back routine.

If the user call-back routine is already in progress, this function does nothing. Otherwise, this function jumps to the call-back defined via USBX_callbackEnable().

Definition at line 254 of file em_usbxpress.c .

Referenced by USBX_DeviceStateChangeCb() , USBX_inXferCompleteCb() , USBX_outXferCompleteCb() , USBX_ResetCb() , and USBX_SetupCmdCb() .

int USBX_outXferCompleteCb ( USB_Status_TypeDef status,
uint16_t xferred,
uint16_t remaining
)

USBXpress OUT Endpoint Transfer Complete Callback.

Gets the number of OUT bytes transferred and passes them to the user API call-back.

Definition at line 282 of file em_usbxpress_callback.c .

References APIEA_GIE , USB_STATUS_OK , USBD_Read() , USBX_jumpCallback() , USBX_RX_COMPLETE , USBX_RX_OVERRUN , USBXCORE_apiEa , USBXCORE_apiIntValue , USBXCORE_byteCountOutPtr , and USBXCORE_readSize .

Referenced by USBX_blockRead() .

void USBX_ResetCb ( void )

USB Reset call-back.

Jump to user API RESET call-back.

Definition at line 54 of file em_usbxpress_callback.c .

References APIEA_GIE , USBX_jumpCallback() , USBX_RESET , USBXCORE_apiEa , USBXCORE_apiIntValue , and USBXCORE_resetState() .

Referenced by USBX_init() .

void USBXCORE_resetState ( void )

Resets internal USBXpress variables.

This function resets the internal USBXpress variables. It should be called after a cancel-type event (USBXpress Close, USB de-configure, FIFO flush, etc.).

Definition at line 266 of file em_usbxpress.c .

References USBXCORE_rxOverflowPacketAvailable , and USBXCORE_zlpActive .

Referenced by USBX_DeviceStateChangeCb() , USBX_ResetCb() , and USBX_SetupCmdCb() .