segmentlcd.c File Reference
EFM32 Segment LCD Display driver.
- Version
- 5.5.0
License
Copyright 2017 Silicon Labs, Inc. www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
segmentlcd.c
.
#include <stdio.h>
#include <string.h>
#include <stdlib.h>
#include <stdbool.h>
#include "
em_device.h
"
#include "
em_cmu.h
"
#include "
em_gpio.h
"
#include "
segmentlcd.h
"
Data Structures |
|
| struct | ARING_TypeDef |
|
Defines segment COM and BIT fields for A-wheel (suited for Anim)
|
|
| struct | ARRAY_TypeDef |
|
Defines segment COM and BIT fields for array.
|
|
| struct | BATTERY_TypeDef |
|
Defines segment COM and BIT fields for Battery (suited for Anim)
|
|
| struct | Block_TypeDef |
|
Defines segment COM and BIT fields for top and bottom row blocks. The bit pattern shown above for characters can be split into upper and lower portions for animation purposes. There are separate COM and BIT numbers which together represent a set of stacked blocks which can be shown on two rows in the segmented LCD screen.
|
|
| struct | CHAR_TypeDef |
|
Defines each text symbol's segment in terms of COM and BIT numbers, in a way that we can enumerate each bit for each text segment in the following bit pattern:
|
|
| struct | EM_TypeDef |
|
Defines segment COM and BIT fields for Energy Modes on display.
|
|
| struct | MCU_DISPLAY |
|
Defines prototype for all segments in display.
|
|
| struct | NUMBER_TypeDef |
|
Defines segment COM and BIT fields numeric display.
|
|
Macros |
|
| #define | ALPHA_DIGITS 7 |
| #define | ALPHA_VAL_MAX 9999999 |
| #define | ALPHA_VAL_MIN -9999999 |
| #define | NUM_DIGITS 4 |
| #define | NUM_VAL_MAX 9999 |
| #define | NUM_VAL_MAX_HEX 0xFFFF |
| #define | NUM_VAL_MIN -999 |
Functions |
|
| static void | displayBlock ( SegmentLCD_BlockMode_TypeDef topMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS], SegmentLCD_BlockMode_TypeDef botMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS]) |
|
Working instance of LCD display.
|
|
| void | SegmentLCD_AllOff (void) |
|
Disable all segments.
|
|
| void | SegmentLCD_AllOn (void) |
|
Enable all segments.
|
|
| void | SegmentLCD_AlphaNumberOff (void) |
|
Turn all segments on alpha characters in display off.
|
|
| void | SegmentLCD_ARing (int anum, int on) |
|
Light up or shut off Ring of Indicators.
|
|
| void | SegmentLCD_Battery (int batteryLevel) |
|
Light up or shut off Battery Indicator.
|
|
| void | SegmentLCD_Block ( SegmentLCD_BlockMode_TypeDef topMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS], SegmentLCD_BlockMode_TypeDef botMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS]) |
| void | SegmentLCD_Disable (void) |
|
Disables LCD controller.
|
|
| void | SegmentLCD_EnergyMode (int em, int on) |
|
Light up or shut off Energy Mode indicator.
|
|
| void | SegmentLCD_Init (bool useBoost) |
|
Segment LCD Initialization routine for EFM32 STK display.
|
|
| void | SegmentLCD_LowerHex (uint32_t num) |
|
Write a hexadecimal number on lower alphanumeric part of Segment LCD display.
|
|
| void | SegmentLCD_LowerNumber (int num) |
|
Write number on lower alphanumeric part of Segment LCD display.
|
|
| void | SegmentLCD_Number (int value) |
|
Write number on numeric part on Segment LCD display.
|
|
| void | SegmentLCD_NumberOff (void) |
|
Turn all segments on numeric digits in display off.
|
|
| unsigned int | SegmentLCD_segCnt (unsigned int segdl, unsigned int segdh) |
|
Counting the number of active segments in a single common line.
|
|
| void | SegmentLCD_Symbol (lcdSymbol s, int on) |
|
Light up or shut off various symbols on Segment LCD.
|
|
| void | SegmentLCD_UnsignedHex (uint32_t value) |
|
Write hexadecimal number on numeric part on Segment LCD display.
|
|
| void | SegmentLCD_Write (const char *string) |
|
Write text on LCD display.
|
|
Variables |
|
| static const uint16_t | Blocks [] |
|
Defines highlighted segments for the block display.
|
|
| static const MCU_DISPLAY | EFM_Display = EFM_DISPLAY_DEF |
|
Working instance of LCD display.
|
|
| static const uint16_t | Segment_Alphabet [] |
|
Defines higlighted segments for the alphabet, starting from "blank" (SPACE) Uses bit pattern as defined for text segments above. E.g. a capital O, would have bits 0 1 2 3 4 5 => 0x003f defined.
|
|
| static const uint16_t | Segment_Numbers [] |
|
Defines higlighted segments for the numeric display.
|
|
Function Documentation
|
static |
Working instance of LCD display.
Enabling/disabling dynamic charge redistribution.
- Parameters
-
true==> enable, false ==> disable
Dynamically switching charge redistribution ON/OFF based on display contents
- Parameters
-
None
Definition at line
1293
of file
segmentlcd.c
.
References Block_TypeDef::bit , Blocks , MCU_DISPLAY::BotBlocks , Block_TypeDef::com , and MCU_DISPLAY::TopBlocks .
| unsigned int SegmentLCD_segCnt | ( | unsigned int |
segdl,
|
| unsigned int |
segdh
|
||
| ) |
Counting the number of active segments in a single common line.
- Parameters
-
valuein registers LCD_SEGDnL and LCD_SEGDnH (n = common line number)
Definition at line
1120
of file
segmentlcd.c
.
Variable Documentation
|
static |
Defines highlighted segments for the block display.
Definition at line
328
of file
segmentlcd.c
.
Referenced by displayBlock() .
|
static |
Defines higlighted segments for the numeric display.
Definition at line
304
of file
segmentlcd.c
.
Referenced by SegmentLCD_Number() , and SegmentLCD_UnsignedHex() .