tftdirect.c File Reference
EFM32GG_DK3750, TFT Initialization and setup for Direct Drive mode.
- Version
- 5.5.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
tftdirect.c
.
#include <stdbool.h>
#include "
em_device.h
"
#include "
em_gpio.h
"
#include "
em_ebi.h
"
#include "
bsp.h
"
#include "
tftdirect.h
"
#include "
glib/glib.h
"
Functions |
|
| void | TFT_DirectGPIOConfig (void) |
|
GPIO configuration for TFT direct drive.
|
|
| bool | TFT_DirectInit (const EBI_TFTInit_TypeDef *tftInit) |
|
TFT initialize or reinitialize Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
|
|
Variables |
|
| static bool | runOnce = true |
Variable Documentation
|
static |
Flag to indicate that we need to initialize once if starting up in
Definition at line
26
of file
tftdirect.c
.
Referenced by TFT_DirectInit() .