CdcKit Drivers
Detailed Description
Implements USB Communication Device Class (CDC).
CDC implementation.
      The source code of the CDC implementation resides in kits/common/drivers/cdc.c and
      
       cdc.h
      
      . This driver implements a basic USB to RS232 bridge.
     
CDC device configuration options.
This section contains a description of the configuration options for the driver. The options are #define's which are expected to be found in the application "usbconfig.h" header file. The values shown below are from the Giant Gecko DK3750 CDC example.
// USB interface numbers. Interfaces are numbered from zero to one less than
// the number of concurrent interfaces supported by the configuration. A CDC
// device is by itself a composite device and has two interfaces.
// The interface numbers must be 0 and 1 for a standalone CDC device, for a
// composite device which includes a CDC interface it must not be in conflict
// with other device interfaces.
#define CDC_CTRL_INTERFACE_NO ( 0 )
#define CDC_DATA_INTERFACE_NO ( 1 )
// Endpoint address for CDC data reception.
#define CDC_EP_DATA_OUT ( 0x01 )
// Endpoint address for CDC data transmission.
#define CDC_EP_DATA_IN ( 0x81 )
// Endpoint address for the notification endpoint (not used).
#define CDC_EP_NOTIFY ( 0x82 )
// Timer id, see USBTIMER in the USB device stack documentation.
// The CDC driver has a Rx timeout functionality which require a timer.
#define CDC_TIMER_ID ( 0 )
// DMA related macros, select DMA channels and DMA request signals.
#define CDC_UART_TX_DMA_CHANNEL   ( 0 )
#define CDC_UART_RX_DMA_CHANNEL   ( 1 )
#define CDC_TX_DMA_SIGNAL         DMAREQ_UART1_TXBL
#define CDC_RX_DMA_SIGNAL         DMAREQ_UART1_RXDATAV
// UART/USART selection macros.
#define CDC_UART                  UART1
#define CDC_UART_CLOCK            cmuClock_UART1
#define CDC_UART_ROUTE            ( UART_ROUTE_RXPEN | UART_ROUTE_TXPEN | \
                                   UART_ROUTE_LOCATION_LOC2 )
#define CDC_UART_TX_PORT          gpioPortB
#define CDC_UART_TX_PIN           9
#define CDC_UART_RX_PORT          gpioPortB
#define CDC_UART_RX_PIN           10
// Activate the RS232 switch on DK's.
#define CDC_ENABLE_DK_UART_SWITCH() BSP_PeripheralAccess(BSP_RS232_UART, true)
// No RS232 switch on STK's. Leave the definition "empty".
#define CDC_ENABLE_DK_UART_SWITCH()
     | Functions | |
| void | CDC_Init (void) | 
| CDC device initialization. | |
| int | CDC_SetupCmd (const USB_Setup_TypeDef *setup) | 
| Handle USB setup commands. Implements CDC class specific commands. | |
| void | CDC_StateChangeEvent ( USBD_State_TypeDef oldState, USBD_State_TypeDef newState) | 
| Callback function called each time the USB device state is changed. Starts CDC operation when device has been configured by USB host. | |
Function Documentation
| int CDC_SetupCmd | ( | const USB_Setup_TypeDef * | 
            setup
            | ) | 
Handle USB setup commands. Implements CDC class specific commands.
- Parameters
- 
         [in] setupPointer to the setup packet received. 
- Returns
- USB_STATUS_OK if command accepted. USB_STATUS_REQ_UNHANDLED when command is unknown, the USB device stack will handle the request.
        Definition at line
        
         183
        
        of file
        
         cdc.c
        
        .
       
References USB_Setup_TypeDef::bRequest , USB_Setup_TypeDef::Direction , USB_Setup_TypeDef::Recipient , USB_Setup_TypeDef::Type , USB_CDC_GETLINECODING , USB_CDC_SETCTRLLINESTATE , USB_CDC_SETLINECODING , USB_SETUP_DIR_IN , USB_SETUP_RECIPIENT_INTERFACE , USB_SETUP_TYPE_CLASS , USB_STATUS_OK , USB_STATUS_REQ_UNHANDLED , USBD_Read() , USBD_Write() , USB_Setup_TypeDef::wIndex , USB_Setup_TypeDef::wLength , and USB_Setup_TypeDef::wValue .
| void CDC_StateChangeEvent | ( | USBD_State_TypeDef | 
            oldState,
            | 
| USBD_State_TypeDef | 
            newState
            | ||
| ) | 
Callback function called each time the USB device state is changed. Starts CDC operation when device has been configured by USB host.
- Parameters
- 
         [in] oldStateThe device state the device has just left. [in] newStateThe new device state. 
        Definition at line
        
         236
        
        of file
        
         cdc.c
        
        .
       
References DMA , DMA_ActivateBasic() , USBD_Read() , USBD_STATE_CONFIGURED , USBD_STATE_SUSPENDED , USBTIMER_Start() , and USBTIMER_Stop() .