EBI_TypeDef Struct ReferenceDevices > EFM32GG_EBI
       Definition at line
       
        48
       
       of file
       
        efm32gg_ebi.h
       
       .
      
| Data Fields | |
| __IOM uint32_t | ADDRTIMING | 
| __IOM uint32_t | ADDRTIMING1 | 
| __IOM uint32_t | ADDRTIMING2 | 
| __IOM uint32_t | ADDRTIMING3 | 
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IM uint32_t | ECCPARITY | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | NANDCTRL | 
| __IOM uint32_t | PAGECTRL | 
| __IOM uint32_t | POLARITY | 
| __IOM uint32_t | POLARITY1 | 
| __IOM uint32_t | POLARITY2 | 
| __IOM uint32_t | POLARITY3 | 
| __IOM uint32_t | RDTIMING | 
| __IOM uint32_t | RDTIMING1 | 
| __IOM uint32_t | RDTIMING2 | 
| __IOM uint32_t | RDTIMING3 | 
| __IOM uint32_t | ROUTE | 
| __IM uint32_t | STATUS | 
| __IOM uint32_t | TFTALPHA | 
| __IOM uint32_t | TFTCTRL | 
| __IOM uint32_t | TFTDD | 
| __IOM uint32_t | TFTFRAMEBASE | 
| __IOM uint32_t | TFTHPORCH | 
| __IOM uint32_t | TFTMASK | 
| __IM uint32_t | TFTPIXEL | 
| __IOM uint32_t | TFTPIXEL0 | 
| __IOM uint32_t | TFTPIXEL1 | 
| __IOM uint32_t | TFTPOLARITY | 
| __IOM uint32_t | TFTSIZE | 
| __IM uint32_t | TFTSTATUS | 
| __IOM uint32_t | TFTSTRIDE | 
| __IOM uint32_t | TFTTIMING | 
| __IOM uint32_t | TFTVPORCH | 
| __IOM uint32_t | WRTIMING | 
| __IOM uint32_t | WRTIMING1 | 
| __IOM uint32_t | WRTIMING2 | 
| __IOM uint32_t | WRTIMING3 | 
Field Documentation
| __IOM uint32_t EBI_TypeDef::ADDRTIMING | 
Address Timing Register
        Definition at line
        
         50
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::ADDRTIMING1 | 
Address Timing Register 1
        Definition at line
        
         55
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::ADDRTIMING2 | 
Address Timing Register 2
        Definition at line
        
         59
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::ADDRTIMING3 | 
Address Timing Register 3
        Definition at line
        
         63
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::CMD | 
Command Register
        Definition at line
        
         69
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::CTRL | 
Control Register
        Definition at line
        
         49
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IM uint32_t EBI_TypeDef::ECCPARITY | 
ECC Parity register
        Definition at line
        
         71
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         90
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IM uint32_t EBI_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         87
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         89
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         88
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::NANDCTRL | 
NAND Control Register
        Definition at line
        
         68
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::PAGECTRL | 
Page Control Register
        Definition at line
        
         67
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::POLARITY | 
Polarity Register
        Definition at line
        
         53
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::POLARITY1 | 
Polarity Register 1
        Definition at line
        
         58
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::POLARITY2 | 
Polarity Register 2
        Definition at line
        
         62
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::POLARITY3 | 
Polarity Register 3
        Definition at line
        
         66
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::RDTIMING | 
Read Timing Register
        Definition at line
        
         51
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::RDTIMING1 | 
Read Timing Register 1
        Definition at line
        
         56
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::RDTIMING2 | 
Read Timing Register 2
        Definition at line
        
         60
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::RDTIMING3 | 
Read Timing Register 3
        Definition at line
        
         64
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::ROUTE | 
I/O Routing Register
        Definition at line
        
         54
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IM uint32_t EBI_TypeDef::STATUS | 
Status Register
        Definition at line
        
         70
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTALPHA | 
TFT Alpha Blending Register
        Definition at line
        
         82
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTCTRL | 
TFT Control Register
        Definition at line
        
         72
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTDD | 
TFT Direct Drive Data Register
        Definition at line
        
         81
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTFRAMEBASE | 
TFT Frame Base Register
        Definition at line
        
         74
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTHPORCH | 
TFT Horizontal Porch Register
        Definition at line
        
         77
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTMASK | 
TFT Masking Register
        Definition at line
        
         86
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IM uint32_t EBI_TypeDef::TFTPIXEL | 
TFT Alpha Blending Result Pixel Register
        Definition at line
        
         85
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTPIXEL0 | 
TFT Pixel 0 Register
        Definition at line
        
         83
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTPIXEL1 | 
TFT Pixel 1 Register
        Definition at line
        
         84
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTPOLARITY | 
TFT Polarity Register
        Definition at line
        
         80
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTSIZE | 
TFT Size Register
        Definition at line
        
         76
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IM uint32_t EBI_TypeDef::TFTSTATUS | 
TFT Status Register
        Definition at line
        
         73
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTSTRIDE | 
TFT Stride Register
        Definition at line
        
         75
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTTIMING | 
TFT Timing Register
        Definition at line
        
         79
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::TFTVPORCH | 
TFT Vertical Porch Register
        Definition at line
        
         78
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::WRTIMING | 
Write Timing Register
        Definition at line
        
         52
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::WRTIMING1 | 
Write Timing Register 1
        Definition at line
        
         57
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::WRTIMING2 | 
Write Timing Register 2
        Definition at line
        
         61
        
        of file
        
         efm32gg_ebi.h
        
        .
       
| __IOM uint32_t EBI_TypeDef::WRTIMING3 | 
Write Timing Register 3
        Definition at line
        
         65
        
        of file
        
         efm32gg_ebi.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG/Include/
       efm32gg_ebi.h