CALIBRATE_TypeDef Struct ReferenceDevices > EFM32GG_CALIBRATE
       Definition at line
       
        49
       
       of file
       
        efm32gg_calibrate.h
       
       .
      
| Data Fields | |
| __IM uint32_t | ADDRESS | 
| __IM uint32_t | VALUE | 
Field Documentation
| __IM uint32_t CALIBRATE_TypeDef::ADDRESS | 
Address of calibration register
        Definition at line
        
         50
        
        of file
        
         efm32gg_calibrate.h
        
        .
       
| __IM uint32_t CALIBRATE_TypeDef::VALUE | 
Default value for calibration register
        Definition at line
        
         51
        
        of file
        
         efm32gg_calibrate.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG/Include/
       efm32gg_calibrate.h