spidrv.c File Reference

SPIDRV API implementation.

Version
5.6.0

License

(C) Copyright 2015 Silicon Labs, www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file spidrv.c.

#include <string.h>
#include "em_device.h"
#include "em_gpio.h"
#include "em_core.h"
#include "em_usart.h"
#include "dmadrv.h"
#include "spidrv.h"

Functions

Ecode_t SPIDRV_AbortTransfer (SPIDRV_Handle_t handle)
 Abort an ongoing SPI transfer.
 
Ecode_t SPIDRV_DeInit (SPIDRV_Handle_t handle)
 Deinitialize an SPI driver instance.
 
Ecode_t SPIDRV_GetBitrate (SPIDRV_Handle_t handle, uint32_t *bitRate)
 Get current SPI bus bitrate.
 
Ecode_t SPIDRV_GetFramelength (SPIDRV_Handle_t handle, uint32_t *frameLength)
 Get current SPI framelength.
 
Ecode_t SPIDRV_GetTransferStatus (SPIDRV_Handle_t handle, int *itemsTransferred, int *itemsRemaining)
 Get the status of an SPI transfer.
 
Ecode_t SPIDRV_Init (SPIDRV_Handle_t handle, SPIDRV_Init_t *initData)
 Initialize an SPI driver instance.
 
Ecode_t SPIDRV_MReceive (SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback)
 Start an SPI master receive transfer.
 
Ecode_t SPIDRV_MReceiveB (SPIDRV_Handle_t handle, void *buffer, int count)
 Start an SPI master blocking receive transfer.
 
Ecode_t SPIDRV_MTransfer (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count, SPIDRV_Callback_t callback)
 Start an SPI master transfer.
 
Ecode_t SPIDRV_MTransferB (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count)
 Start an SPI master blocking transfer.
 
Ecode_t SPIDRV_MTransferSingleItemB (SPIDRV_Handle_t handle, uint32_t txValue, void *rxValue)
 Start an SPI master blocking single item (frame) transfer.
 
Ecode_t SPIDRV_MTransmit (SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback)
 Start an SPI master transmit transfer.
 
Ecode_t SPIDRV_MTransmitB (SPIDRV_Handle_t handle, const void *buffer, int count)
 Start an SPI master blocking transmit transfer.
 
Ecode_t SPIDRV_SetBitrate (SPIDRV_Handle_t handle, uint32_t bitRate)
 Set SPI bus bitrate.
 
Ecode_t SPIDRV_SetFramelength (SPIDRV_Handle_t handle, uint32_t frameLength)
 Set SPI framelength.
 
Ecode_t SPIDRV_SReceive (SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs)
 Start an SPI slave receive transfer.
 
Ecode_t SPIDRV_SReceiveB (SPIDRV_Handle_t handle, void *buffer, int count, int timeoutMs)
 Start an SPI slave blocking receive transfer.
 
Ecode_t SPIDRV_STransfer (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count, SPIDRV_Callback_t callback, int timeoutMs)
 Start an SPI slave transfer.
 
Ecode_t SPIDRV_STransferB (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count, int timeoutMs)
 Start an SPI slave blocking transfer.
 
Ecode_t SPIDRV_STransmit (SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs)
 Start an SPI slave transmit transfer.
 
Ecode_t SPIDRV_STransmitB (SPIDRV_Handle_t handle, const void *buffer, int count, int timeoutMs)
 Start an SPI slave blocking transmit transfer.