Unmod_Carrier_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Unmodulated Carrier plugin, see Plugin System Layer for detailed documentation.
.
Data Structures |
|
| struct | EZRADIODRV_UnmodCarrierHandle |
|
EzRadio unmodulated carrier plug-in instance initialization and handler structure.
|
|
Macros |
|
| #define | EZRADIODRV_UNMOD_CARRIER_PLUGIN_INIT_DEFAULT |
|
Configuration data for EzRadio unmodulated carrier plug-in.
|
|
Typedefs |
|
| typedef struct EZRADIODRV_UnmodCarrierHandle | EZRADIODRV_UnmodCarrierHandle_t |
|
EzRadio unmodulated carrier plug-in instance initialization and handler structure.
|
|
Functions |
|
| Ecode_t | ezradioStartUnmodulatedCarrier ( EZRADIODRV_Handle_t radioHandle) |
|
Starts unmodulated carrier transmission with the radio configurations from the radioHandle parameter.
|
|
| Ecode_t | ezradioStopUnmodulatedCarrier (void) |
|
Stops unmodulated carrier transmission.
|
|
Macro Definition Documentation
| #define EZRADIODRV_UNMOD_CARRIER_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio unmodulated carrier plug-in.
Definition at line
73
of file
ezradio_unmod_carrier_plugin.h
.
Function Documentation
| Ecode_t ezradioStartUnmodulatedCarrier | ( | EZRADIODRV_Handle_t |
radioHandle
|
) |
Starts unmodulated carrier transmission with the radio configurations from the radioHandle parameter.
- Parameters
-
radioHandleHandler of the EzRadio driver instance where channel configuration is set.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
56
of file
ezradio_unmod_carrier_plugin.c
.
References EZRADIODRV_UnmodCarrierHandle::channel , ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED , ezradio_get_int_status() , ezradio_request_device_state() , ezradio_start_tx() , and EZRADIODRV_HandleData::unmodCarrier .
| Ecode_t ezradioStopUnmodulatedCarrier | ( | void |
|
) |
Stops unmodulated carrier transmission.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
87
of file
ezradio_unmod_carrier_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_OK , and ezradio_change_state() .