WDOGEMLIB
Detailed Description
Watchdog (WDOG) Peripheral API.
This module contains functions to control the WDOG peripheral of Silicon Labs 32-bit MCUs and SoCs. The WDOG resets the system in case of a fault condition.
Data Structures | |
struct | WDOG_Init_TypeDef |
Macros | |
#define | DEFAULT_WDOG WDOG |
#define | WDOG_INIT_DEFAULT |
Enumerations | |
enum | WDOG_ClkSel_TypeDef { wdogClkSelULFRCO = _WDOG_CTRL_CLKSEL_ULFRCO, wdogClkSelLFRCO = _WDOG_CTRL_CLKSEL_LFRCO, wdogClkSelLFXO = _WDOG_CTRL_CLKSEL_LFXO } |
enum | WDOG_PeriodSel_TypeDef { wdogPeriod_9 = 0x0, wdogPeriod_17 = 0x1, wdogPeriod_33 = 0x2, wdogPeriod_65 = 0x3, wdogPeriod_129 = 0x4, wdogPeriod_257 = 0x5, wdogPeriod_513 = 0x6, wdogPeriod_1k = 0x7, wdogPeriod_2k = 0x8, wdogPeriod_4k = 0x9, wdogPeriod_8k = 0xA, wdogPeriod_16k = 0xB, wdogPeriod_32k = 0xC, wdogPeriod_64k = 0xD, wdogPeriod_128k = 0xE, wdogPeriod_256k = 0xF } |
Functions | |
__STATIC_INLINE void | WDOG_Enable (bool enable) |
Enable/disable the watchdog timer. | |
__STATIC_INLINE void | WDOG_Feed (void) |
Feed the watchdog. | |
__STATIC_INLINE void | WDOG_Init (const WDOG_Init_TypeDef *init) |
Initialize watchdog (assuming the watchdog configuration has not been locked). | |
__STATIC_INLINE bool | WDOG_IsEnabled (void) |
Get enabled status of the watchdog. | |
__STATIC_INLINE bool | WDOG_IsLocked (void) |
Get locked status of the watchdog. | |
__STATIC_INLINE void | WDOG_Lock (void) |
Lock the watchdog configuration. | |
void | WDOGn_Enable (WDOG_TypeDef *wdog, bool enable) |
Enable/disable the watchdog timer. | |
void | WDOGn_Feed (WDOG_TypeDef *wdog) |
Feed WDOG. | |
void | WDOGn_Init (WDOG_TypeDef *wdog, const WDOG_Init_TypeDef *init) |
Initialize WDOG (assuming the WDOG configuration has not been locked). | |
__STATIC_INLINE bool | WDOGn_IsEnabled (WDOG_TypeDef *wdog) |
Get enabled status of the watchdog. | |
__STATIC_INLINE bool | WDOGn_IsLocked (WDOG_TypeDef *wdog) |
Get locked status of the watchdog. | |
void | WDOGn_Lock (WDOG_TypeDef *wdog) |
Lock the WDOG configuration. | |
void | WDOGn_Unlock (WDOG_TypeDef *wdog) |
Unlock the WDOG configuration. | |
Macro Definition Documentation
#define DEFAULT_WDOG WDOG |
Default WDOG instance for deprecated functions.
Definition at line 64
of file em_wdog.h
.
Referenced by WDOG_Enable(), WDOG_Feed(), WDOG_Init(), WDOG_IsEnabled(), WDOG_IsLocked(), and WDOG_Lock().
#define WDOG_INIT_DEFAULT |
Suggested default configuration for WDOG initialization structure.
Definition at line 217
of file em_wdog.h
.
Enumeration Type Documentation
enum WDOG_ClkSel_TypeDef |
Watchdog period selection.
Definition at line 82
of file em_wdog.h
.
Function Documentation
__STATIC_INLINE void WDOG_Enable | ( | bool | enable | ) |
Enable/disable the watchdog timer.
Deprecated:
- Deprecated function. New code should use WDOGn_Enable(). This function uses DEFAULT_WDOG.
- Parameters
-
[in] enable
Set to true to enable watchdog, false to disable. Watchdog cannot be disabled if watchdog has been locked.
Definition at line 415
of file em_wdog.h
.
References DEFAULT_WDOG, and WDOGn_Enable().
__STATIC_INLINE void WDOG_Feed | ( | void |
| ) |
Feed the watchdog.
Deprecated:
- Deprecated function. New code should use WDOGn_Feed(). This function uses DEFAULT_WDOG.
Definition at line 428
of file em_wdog.h
.
References DEFAULT_WDOG, and WDOGn_Feed().
__STATIC_INLINE void WDOG_Init | ( | const WDOG_Init_TypeDef * | init | ) |
Initialize watchdog (assuming the watchdog configuration has not been locked).
Deprecated:
- Deprecated function. New code should use WDOGn_Init(). This function uses DEFAULT_WDOG.
- Parameters
-
[in] init
Structure holding watchdog configuration. A default setting WDOG_INIT_DEFAULT is available for initialization.
Definition at line 446
of file em_wdog.h
.
References DEFAULT_WDOG, and WDOGn_Init().
__STATIC_INLINE bool WDOG_IsEnabled | ( | void |
| ) |
Get enabled status of the watchdog.
Deprecated:
- Deprecated function. New code should use WDOGn_IsEnabled(). This function uses DEFAULT_WDOG.
Definition at line 472
of file em_wdog.h
.
References DEFAULT_WDOG, and WDOGn_IsEnabled().
__STATIC_INLINE bool WDOG_IsLocked | ( | void |
| ) |
Get locked status of the watchdog.
Deprecated:
- Deprecated function. New code should use WDOGn_IsLocked(). This function uses DEFAULT_WDOG.
Definition at line 485
of file em_wdog.h
.
References DEFAULT_WDOG, and WDOGn_IsLocked().
__STATIC_INLINE void WDOG_Lock | ( | void |
| ) |
Lock the watchdog configuration.
Deprecated:
- Deprecated function. New code should use WDOGn_Lock(). This function uses DEFAULT_WDOG.
Definition at line 459
of file em_wdog.h
.
References DEFAULT_WDOG, and WDOGn_Lock().
void WDOGn_Enable | ( | WDOG_TypeDef * | wdog, |
bool | enable |
||
) |
Enable/disable the watchdog timer.
- Note
- This function modifies the WDOG CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.
- Parameters
-
[in] wdog
A pointer to the WDOG peripheral register block. [in] enable
True to enable Watchdog, false to disable. Watchdog cannot be disabled if it's been locked.
Definition at line 76
of file em_wdog.c
.
References _WDOG_CTRL_EN_SHIFT, BUS_RegBitRead(), BUS_RegBitWrite(), WDOG_TypeDef::CTRL, WDOG_TypeDef::SYNCBUSY, WDOG_CTRL_LOCK, WDOG_SYNCBUSY_CMD, and WDOG_SYNCBUSY_CTRL.
Referenced by WDOG_Enable(), and WDOGn_Init().
void WDOGn_Feed | ( | WDOG_TypeDef * | wdog | ) |
Feed WDOG.
When WDOG is activated, it must be fed (i.e., clearing the counter) before it reaches the defined timeout period. Otherwise, WDOG will generate a reset.
- Parameters
-
[in] wdog
A pointer to the WDOG peripheral register block.
Definition at line 126
of file em_wdog.c
.
References WDOG_TypeDef::CMD, CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, CORE_EXIT_ATOMIC, WDOG_TypeDef::CTRL, WDOG_TypeDef::SYNCBUSY, WDOG_CMD_CLEAR, WDOG_CTRL_EN, WDOG_SYNCBUSY_CMD, and WDOG_SYNCBUSY_CTRL.
Referenced by WDOG_Feed().
void WDOGn_Init | ( | WDOG_TypeDef * | wdog, |
const WDOG_Init_TypeDef * | init |
||
) |
Initialize WDOG (assuming the WDOG configuration has not been locked).
- Note
- This function modifies the WDOG CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.
- Parameters
-
[in] wdog
Pointer to the WDOG peripheral register block. [in] init
The structure holding the WDOG configuration. A default setting WDOG_INIT_DEFAULT is available for initialization.
Definition at line 188
of file em_wdog.c
.
References _WDOG_CTRL_CLKSEL_SHIFT, _WDOG_CTRL_PERSEL_SHIFT, WDOG_Init_TypeDef::clkSel, WDOG_TypeDef::CTRL, WDOG_Init_TypeDef::debugRun, WDOG_Init_TypeDef::em2Run, WDOG_Init_TypeDef::em3Run, WDOG_Init_TypeDef::em4Block, WDOG_Init_TypeDef::enable, WDOG_Init_TypeDef::lock, WDOG_Init_TypeDef::perSel, WDOG_Init_TypeDef::swoscBlock, WDOG_TypeDef::SYNCBUSY, WDOG_CTRL_DEBUGRUN, WDOG_CTRL_EM2RUN, WDOG_CTRL_EM3RUN, WDOG_CTRL_EM4BLOCK, WDOG_CTRL_EN, WDOG_CTRL_LOCK, WDOG_CTRL_SWOSCBLOCK, WDOG_SYNCBUSY_CTRL, WDOGn_Enable(), and WDOGn_Lock().
Referenced by WDOG_Init().
__STATIC_INLINE bool WDOGn_IsEnabled | ( | WDOG_TypeDef * | wdog | ) |
Get enabled status of the watchdog.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block.
Definition at line 378
of file em_wdog.h
.
References _WDOG_CTRL_EN_MASK, WDOG_TypeDef::CTRL, and WDOG_CTRL_EN.
Referenced by WDOG_IsEnabled().
__STATIC_INLINE bool WDOGn_IsLocked | ( | WDOG_TypeDef * | wdog | ) |
Get locked status of the watchdog.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block.
Definition at line 394
of file em_wdog.h
.
References _WDOG_CTRL_LOCK_MASK, WDOG_TypeDef::CTRL, and WDOG_CTRL_LOCK.
Referenced by WDOG_IsLocked().
void WDOGn_Lock | ( | WDOG_TypeDef * | wdog | ) |
Lock the WDOG configuration.
This prevents errors from overwriting the WDOG configuration, possibly disabling it. Only a reset can unlock the WDOG configuration once locked.
If the LFRCO or LFXO clocks are used to clock WDOG, consider using the option of inhibiting those clocks to be disabled. See the WDOG_Enable() initialization structure.
- Note
- This function modifies the WDOG CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.
- Parameters
-
[in] wdog
A pointer to WDOG peripheral register block.
Definition at line 269
of file em_wdog.c
.
References _WDOG_CTRL_LOCK_SHIFT, BUS_RegBitWrite(), WDOG_TypeDef::CTRL, WDOG_TypeDef::SYNCBUSY, and WDOG_SYNCBUSY_CTRL.
Referenced by WDOG_Lock(), and WDOGn_Init().
void WDOGn_Unlock | ( | WDOG_TypeDef * | wdog | ) |
Unlock the WDOG configuration.
Note that this function will have no effect on devices where a reset is the only way to unlock the watchdog.
- Parameters
-
[in] wdog
A pointer to WDOG peripheral register block.
Definition at line 295
of file em_wdog.c
.