NORFLASH_Info_TypeDef Struct ReferenceKit Drivers > NorFlash
NORFLASH device information struct.
Definition at line 49
of file norflash.h
.
#include <
norflash.h
>
Data Fields | |
uint32_t | baseAddress |
uint32_t | deviceId |
uint32_t | deviceSize |
uint16_t | manufacturerId |
uint32_t | sectorCount |
uint32_t | sectorSize |
Field Documentation
uint32_t NORFLASH_Info_TypeDef::baseAddress |
The device base address in cpu memory map.
Definition at line 50
of file norflash.h
.
Referenced by NORFLASH_AddressValid(), and NORFLASH_EraseDevice().
uint32_t NORFLASH_Info_TypeDef::deviceId |
The device ID.
Definition at line 51
of file norflash.h
.
uint32_t NORFLASH_Info_TypeDef::deviceSize |
Total device size in bytes.
Definition at line 52
of file norflash.h
.
Referenced by NORFLASH_AddressValid().
uint16_t NORFLASH_Info_TypeDef::manufacturerId |
The device manufacturer ID.
Definition at line 55
of file norflash.h
.
uint32_t NORFLASH_Info_TypeDef::sectorCount |
Number of sectors in the device.
Definition at line 53
of file norflash.h
.
uint32_t NORFLASH_Info_TypeDef::sectorSize |
Sector size in bytes.
Definition at line 54
of file norflash.h
.
Referenced by NORFLASH_EraseSector(), and NORFLASH_Program().
The documentation for this struct was generated from the following files:
- C:/repos/embsw_super_h1/hardware/kit/common/drivers/
norflash.h
- C:/repos/embsw_super_h1/hardware/kit/common/drivers/
norflash_s29gl.h