ezradio_direct_transmit_plugin.c File Reference

EzRadio direct transmission plug-in managed by the plug-in manager if enabled.

License

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

Definition in file ezradio_direct_transmit_plugin.c .

#include <stddef.h>
#include " em_device.h "
#include "ezradio_cmd.h"
#include "ezradio_prop.h"
#include " ezradio_api_lib.h "
#include "ezradio_api_lib_add.h"
#include " ezradio_plugin_manager.h "
#include " ezradio_transmit_plugin.h "

Functions

Ecode_t ezradioStartDirectTransmit ( EZRADIODRV_Handle_t radioHandle)
Starts direct transmission with the radio configurations from the radioHandle parameter.
Ecode_t ezradioStopDirectTransmit (void)
Stops direct transmission.