RMUEMLIB
Detailed Description
Reset Management Unit (RMU) Peripheral API.
This module contains functions to control the RMU peripheral of Silicon Labs 32-bit MCUs and SoCs. RMU ensures correct reset operation and is responsible for connecting the different reset sources to the reset lines of the MCU or SoC.
Macros | |
#define | RMU_LockupResetDisable(A) RMU_ResetControl(rmuResetLockUp, A) |
Enumerations | |
enum | RMU_Reset_TypeDef { rmuResetLockUp = _RMU_CTRL_LOCKUPRDIS_MASK } |
enum | RMU_ResetMode_TypeDef { rmuResetModeClear = 0, rmuResetModeSet = 1 } |
Functions | |
void | RMU_ResetCauseClear (void) |
Clear the reset cause register. | |
uint32_t | RMU_ResetCauseGet (void) |
Get the cause of the last reset. | |
void | RMU_ResetControl (RMU_Reset_TypeDef reset, RMU_ResetMode_TypeDef mode) |
Disable/enable reset for various peripherals and signal sources. | |
Macro Definition Documentation
#define RMU_LockupResetDisable | ( | A | ) | RMU_ResetControl(rmuResetLockUp, A) |
RMU_LockupResetDisable kept for backwards compatibility.
Definition at line 132
of file em_rmu.h
.
Enumeration Type Documentation
enum RMU_Reset_TypeDef |
RMU reset modes.
Definition at line 60
of file em_rmu.h
.
Function Documentation
void RMU_ResetCauseClear | ( | void |
| ) |
Clear the reset cause register.
This function clears all the reset cause bits of the RSTCAUSE register. The reset cause bits must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseGet().
Definition at line 274
of file em_rmu.c
.
References _EMU_AUXCTRL_HRCCLR_SHIFT, BUS_RegBitWrite(), EMU, EMU_Lock(), EMU_LOCK_LOCKKEY_LOCKED, EMU_Unlock(), RMU, and RMU_CMD_RCCLR.
Referenced by SLEEP_Init().
uint32_t RMU_ResetCauseGet | ( | void |
| ) |
Get the cause of the last reset.
To be useful, the reset cause must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseClear(). This function call will return the main cause for reset, which can be a bit mask (several causes) and clear away "noise".
- Returns
- A reset cause mask. See the reference manual for a description of the reset cause mask.
Definition at line 317
of file em_rmu.c
.
References EMU, EMU_BASE, RMU, RMU_RSTCAUSE_EM4RST, RMU_RSTCAUSE_EXTRST, RMU_RSTCAUSE_LOCKUPRST, RMU_RSTCAUSE_SYSREQRST, and RMU_RSTCAUSE_WDOGRST.
Referenced by SLEEP_Init().
void RMU_ResetControl | ( | RMU_Reset_TypeDef | reset, |
RMU_ResetMode_TypeDef | mode |
||
) |
Disable/enable reset for various peripherals and signal sources.
- Parameters
-
[in] reset
Reset types to enable/disable.s [in] mode
Reset mode.
Definition at line 246
of file em_rmu.c
.
References BUS_RegBitWrite(), EMU, RMU, and SL_CTZ().