DAC_InitChannel_TypeDef Struct ReferenceEMLIB > DAC
DAC channel initialization structure.
Definition at line 185
of file em_dac.h
.
#include <
em_dac.h
>
Data Fields | |
bool | enable |
bool | prsEnable |
DAC_PRSSEL_TypeDef | prsSel |
bool | refreshEnable |
Field Documentation
bool DAC_InitChannel_TypeDef::enable |
bool DAC_InitChannel_TypeDef::prsEnable |
Peripheral reflex system trigger enable. If false, channel is triggered by writing to CHnDATA.
Definition at line 193
of file em_dac.h
.
Referenced by DAC_InitChannel().
DAC_PRSSEL_TypeDef DAC_InitChannel_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if prsEnable
is enabled.
Definition at line 206
of file em_dac.h
.
Referenced by DAC_InitChannel().
bool DAC_InitChannel_TypeDef::refreshEnable |
Enable/disable automatic refresh of channel. Refresh interval must be defined in common control initialization, see DAC_Init() for more information.
Definition at line 200
of file em_dac.h
.
Referenced by DAC_InitChannel().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emlib/inc/
em_dac.h