ezradio_plugin_manager.c File Reference
This file contains the plug-in manager for the EZRadio and.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
- The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
- Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
- This notice may not be removed or altered from any source distribution.
Definition in file ezradio_plugin_manager.c
.
#include <stddef.h>
#include <stdio.h>
#include <stdbool.h>
#include "em_gpio.h
"
#include "gpiointerrupt.h
"
#include "ustimer.h
"
#include "ezradio_cmd.h"
#include "ezradio_prop.h"
#include "ezradio_hal.h
"
#include "ezradio_api_lib.h
"
#include "ezradio_api_lib_add.h"
#include "ezradio_plugin_manager.h
"
Functions | |
void | ezradioInit (EZRADIODRV_Handle_t handle) |
Radio Initialization. | |
Ecode_t | ezradioPluginManager (EZRADIODRV_Handle_t radioHandle) |
EzRadio plugin manager state machine handler. This function should be called in the application in an infinite loop, in order to manage the EzRadio plug-ins properly. | |
void | ezradioResetTRxFifo (void) |
Resets both the TX and RX FIFOs. | |