EMU_DCDCInit_TypeDef Struct ReferenceEMLIB > EMU

DCDC regulator initialization structure.

Definition at line 739 of file em_emu.h .

#include < em_emu.h >

Data Fields

EMU_VreginCmpThreshold_TypeDef cmpThreshold
bool dcmOnlyEn
EMU_DcdcDriveSpeed_TypeDef driveSpeedEM01
EMU_DcdcDriveSpeed_TypeDef driveSpeedEM23
EMU_DcdcMode_TypeDef mode
EMU_DcdcPeakCurrent_TypeDef peakCurrentEM01
EMU_DcdcPeakCurrent_TypeDef peakCurrentEM23
EMU_DcdcTonMaxTimeout_TypeDef tonMax

Field Documentation

EMU_VreginCmpThreshold_TypeDef EMU_DCDCInit_TypeDef::cmpThreshold

VREGIN comparator threshold.

Definition at line 741 of file em_emu.h .

bool EMU_DCDCInit_TypeDef::dcmOnlyEn

DCM only mode enable.

Definition at line 743 of file em_emu.h .

EMU_DcdcDriveSpeed_TypeDef EMU_DCDCInit_TypeDef::driveSpeedEM01

DCDC drive speed in EM0/1.

Definition at line 744 of file em_emu.h .

EMU_DcdcDriveSpeed_TypeDef EMU_DCDCInit_TypeDef::driveSpeedEM23

DCDC drive speed in EM2/3.

Definition at line 745 of file em_emu.h .

EMU_DcdcMode_TypeDef EMU_DCDCInit_TypeDef::mode

DCDC mode.

Definition at line 740 of file em_emu.h .

Referenced by BSP_initDcdc() .

EMU_DcdcPeakCurrent_TypeDef EMU_DCDCInit_TypeDef::peakCurrentEM01

EM0/1 peak current setting.

Definition at line 746 of file em_emu.h .

EMU_DcdcPeakCurrent_TypeDef EMU_DCDCInit_TypeDef::peakCurrentEM23

EM2/3 peak current setting.

Definition at line 747 of file em_emu.h .

EMU_DcdcTonMaxTimeout_TypeDef EMU_DCDCInit_TypeDef::tonMax

Ton max timeout control.

Definition at line 742 of file em_emu.h .


The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emlib/inc/ em_emu.h