SYSTEM_CalAddrVal_TypeDef Struct ReferenceEMLIB > SYSTEM

DEVINFO calibration address/value pair.

Definition at line 292 of file em_system.h .

#include < em_system.h >

Data Fields

uint32_t address
uint32_t calValue

Field Documentation

uint32_t SYSTEM_CalAddrVal_TypeDef::address

Peripheral calibration register address.

Definition at line 293 of file em_system.h .

Referenced by SYSTEM_GetCalibrationValue() .

uint32_t SYSTEM_CalAddrVal_TypeDef::calValue

Calibration value for register at address.

Definition at line 294 of file em_system.h .

Referenced by SYSTEM_GetCalibrationValue() .


The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emlib/inc/ em_system.h