IADC_SingleInput_t Struct ReferenceEMLIB > IADC

IADC single input selection structure

Definition at line 748 of file em_iadc.h .

#include < em_iadc.h >

Data Fields

bool compare
uint8_t configId
IADC_NegInput_t negInput
IADC_PosInput_t posInput

Field Documentation

bool IADC_SingleInput_t::compare

Perform digital window comparison on the result from this entry.

Definition at line 752 of file em_iadc.h .

Referenced by IADC_updateSingleInput() .

uint8_t IADC_SingleInput_t::configId

Configuration id.

Definition at line 751 of file em_iadc.h .

Referenced by IADC_updateSingleInput() .

IADC_NegInput_t IADC_SingleInput_t::negInput

Port/pin input for the negative side of the ADC.

Definition at line 749 of file em_iadc.h .

Referenced by IADC_updateSingleInput() .

IADC_PosInput_t IADC_SingleInput_t::posInput

Port/pin input for the positive side of the ADC.

Definition at line 750 of file em_iadc.h .

Referenced by IADC_updateSingleInput() .


The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emlib/inc/ em_iadc.h