TOUCH_Pos_TypeDef Struct ReferenceKit Drivers > Touch

Touch panel position structure

Definition at line 60 of file touch.h .

#include < touch.h >

Data Fields

uint16_t adcx
uint16_t adcy
uint8_t pen
uint16_t x
uint16_t y

Field Documentation

uint16_t TOUCH_Pos_TypeDef::adcx

ADC X readings

Definition at line 63 of file touch.h .

Referenced by ADC0_IRQHandler() , TOUCH_GetPos() , and TOUCH_RecalculatePosition() .

uint16_t TOUCH_Pos_TypeDef::adcy

ADC Y readings

Definition at line 64 of file touch.h .

Referenced by ADC0_IRQHandler() , TOUCH_GetPos() , and TOUCH_RecalculatePosition() .

uint8_t TOUCH_Pos_TypeDef::pen

0=not pressed, 1=touched

Definition at line 65 of file touch.h .

Referenced by ADC0_IRQHandler() , TOUCH_GetPos() , TOUCH_RecalculatePosition() , and TOUCH_StateChanged() .

uint16_t TOUCH_Pos_TypeDef::x

x position

Definition at line 61 of file touch.h .

Referenced by ADC0_IRQHandler() , TOUCH_GetPos() , TOUCH_RecalculatePosition() , and TOUCH_StateChanged() .

uint16_t TOUCH_Pos_TypeDef::y

y position

Definition at line 62 of file touch.h .

Referenced by ADC0_IRQHandler() , TOUCH_GetPos() , TOUCH_RecalculatePosition() , and TOUCH_StateChanged() .


The documentation for this struct was generated from the following file:
  • C:/repos/super/hardware/kit/common/drivers/ touch.h