__BMP_DataType Struct ReferencePlatform Middleware > GLIB

BMP Data type structure to hold information about the bmp data returned.

Definition at line 142 of file bmp.h .

#include < bmp.h >

Data Fields

uint16_t bitsPerPixel
uint32_t compressionType
uint32_t endOfRow
uint32_t size

Field Documentation

uint16_t __BMP_DataType::bitsPerPixel

Color depth of the data returned from function.

Definition at line 144 of file bmp.h .

Referenced by BMP_readRawData() , BMP_readRawData24bit() , BMP_readRawData8bit() , and BMP_readRawDataRLE8() .

uint32_t __BMP_DataType::compressionType

Compression type

Definition at line 146 of file bmp.h .

Referenced by BMP_readRawData() , BMP_readRawData24bit() , BMP_readRawData8bit() , and BMP_readRawDataRLE8() .

uint32_t __BMP_DataType::endOfRow

Marks whether this data is at the end of the current row. endOfRow == 1, if end of row is reached. endOfRow == 0, if there is still unread data left in the row

Definition at line 150 of file bmp.h .

Referenced by BMP_readRawData() , BMP_readRawData24bit() , BMP_readRawData8bit() , BMP_readRawDataRLE8() , BMP_readRgbData() , BMP_readRgbDataRLE8() , and BMP_readRleData() .

uint32_t __BMP_DataType::size

Byte length of returned data

Definition at line 148 of file bmp.h .

Referenced by BMP_readRawData() , BMP_readRawData24bit() , BMP_readRawData8bit() , BMP_readRawDataRLE8() , and BMP_readRgbData() .


The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/middleware/glib/glib/ bmp.h