IADC_InitScan_t Struct ReferenceEMLIB > IADC

IADC scan init structure

Definition at line 699 of file em_iadc.h.

#include <em_iadc.h>

Data Fields

IADC_Alignment_t alignment
 
uint8_t dataValidLevel
 
bool fifoDmaWakeup
 
bool showId
 
bool start
 
IADC_TriggerAction_t triggerAction
 
IADC_TriggerSel_t triggerSelect
 

Field Documentation

IADC_Alignment_t IADC_InitScan_t::alignment

Alignment of data in FIFO.

Definition at line 700 of file em_iadc.h.

Referenced by IADC_initScan().

uint8_t IADC_InitScan_t::dataValidLevel

Data valid level before requesting DMA transfer.

Definition at line 702 of file em_iadc.h.

Referenced by IADC_initScan().

bool IADC_InitScan_t::fifoDmaWakeup

Wake-up DMA when FIFO reaches data valid level.

Definition at line 703 of file em_iadc.h.

Referenced by IADC_initScan().

bool IADC_InitScan_t::showId

Tag FIFO entry with scan table entry id.

Definition at line 701 of file em_iadc.h.

Referenced by IADC_initScan().

bool IADC_InitScan_t::start

Start scan immediately.

Definition at line 706 of file em_iadc.h.

Referenced by IADC_initScan().

IADC_TriggerAction_t IADC_InitScan_t::triggerAction

Trigger action.

Definition at line 705 of file em_iadc.h.

Referenced by IADC_initScan().

IADC_TriggerSel_t IADC_InitScan_t::triggerSelect

Trigger selection.

Definition at line 704 of file em_iadc.h.

Referenced by IADC_initScan().


The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emlib/inc/em_iadc.h