root_OutputMailbox_t Struct ReferenceEMLIB > SE
Definition at line 98
of file em_se.c
.
Data Fields | |
volatile uint32_t | command |
volatile uint32_t | data [0] |
volatile uint32_t | length |
volatile uint32_t | magic |
volatile uint32_t | status |
volatile uint32_t | version |
The documentation for this struct was generated from the following file:
- C:/repos/super/platform/emlib/src/
em_se.c