Receive_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Receive plugin, see Plugin System Layer for detailed documentation.
.
Data Structures | |
struct | EZRADIODRV_PacketRxHandle |
EzRadio receive plug-in instance initialization and handler structure. | |
Macros | |
#define | EZRADIODRV_RECEIVE_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio receive plug-in. | |
Typedefs | |
typedef struct EZRADIODRV_PacketRxHandle | EZRADIODRV_PacketRxHandle_t |
EzRadio receive plug-in instance initialization and handler structure. | |
Functions | |
Ecode_t | ezradioStartRx (EZRADIODRV_Handle_t radioHandle) |
Set Radio to RX mode, packet length is always coming from the radio configuration. | |
Macro Definition Documentation
#define EZRADIODRV_RECEIVE_PLUGIN_INIT_DEFAULT |
Value:
{ /* Packet RX */ \
NULL, /* CallBack */ \
RADIO_CONFIGURATION_DATA_CHANNEL_NUMBER, /* Channel */ \
NULL, /* Packet buffer */ \
},
Configuration data for EzRadio receive plug-in.
Definition at line 72
of file ezradio_receive_plugin.h
.
Function Documentation
Ecode_t ezradioStartRx | ( | EZRADIODRV_Handle_t | radioHandle | ) |
Set Radio to RX mode, packet length is always coming from the radio configuration.
- Parameters
-
radioHandle
Handler of the EzRadio driver instance where packet buffer, callback and channel configurations are set.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line 62
of file ezradio_receive_plugin.c
.
References EZRADIODRV_PacketRxHandle::channel, ECODE_EMDRV_EZRADIODRV_OK, ezradio_start_rx(), and EZRADIODRV_HandleData::packetRx.