INTEMLIB
Detailed Description
Safe nesting of interrupt disable/enable API.
Deprecated:
- These functions are deprecated and marked for removal in a later release. Use the CORE module instead. See Porting from em_int for information on how to convert existing code bases to use CORE.
This module contains functions to safely disable and enable interrupts at the CPU level. INT_Disable() disables interrupts globally and increments a lock level counter (counting semaphore). INT_Enable() decrements the lock level counter and enables interrupts if the counter reaches zero.
These functions would normally be used to secure critical regions and to make sure that a critical section that calls into another critical section does not unintentionally terminate the callee critical section.
These functions should also be used inside interrupt handlers:
* void SysTick_Handler(void) * { * INT_Disable(); * . * . * . * INT_Enable(); * } *
Functions | |
__STATIC_INLINE uint32_t | INT_Disable (void) |
Disable interrupts. | |
__STATIC_INLINE uint32_t | INT_Enable (void) |
Enable interrupts. | |
Variables | |
uint32_t | INT_LockCnt = 0 |
Function Documentation
__STATIC_INLINE uint32_t INT_Disable | ( | void |
| ) |
Disable interrupts.
Deprecated:
- Deprecated and marked for removal in a later release. Use new CORE module instead.
Disable interrupts and increment lock level counter.
- Returns
- Resulting interrupt disable nesting level.
Definition at line 76
of file em_int.h
.
References INT_LockCnt.
__STATIC_INLINE uint32_t INT_Enable | ( | void |
| ) |
Enable interrupts.
Deprecated:
- Deprecated and marked for removal in a later release. Use the new CORE module instead.
- Returns
- Resulting interrupt disable nesting level.
Decrement interrupt lock level counter and enable interrupts if counter reached zero.
Definition at line 102
of file em_int.h
.
References INT_LockCnt.
Variable Documentation
uint32_t INT_LockCnt = 0 |
An interrupt lock level counter. Set to zero initially because main is normally entered with interrupts enabled.
Definition at line 73
of file em_int.c
.
Referenced by INT_Disable(), and INT_Enable().