Direct_Receive_PluginEMDRV > EZRADIODRV > Plugin_System

Detailed Description

Direct receive plugin, see Plugin System Layer for detailed documentation.


     

.

Data Structures

struct EZRADIODRV_DirectRxHandle
EzRadio direct rx plug-in instance initialization and handler structure.

Macros

#define EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT
Configuration data for EzRadio direct rx plug-in.

Typedefs

typedef struct EZRADIODRV_DirectRxHandle EZRADIODRV_DirectRxHandle_t
EzRadio direct rx plug-in instance initialization and handler structure.

Functions

Ecode_t ezradioStartDirectReceive ( EZRADIODRV_Handle_t radioHandle)
Starts direct reception with the radio configurations from the radioHandle parameter.
Ecode_t ezradioStopDirectReceive (void)
Stops direct reception.

Macro Definition Documentation

#define EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT
Value:
{ /* PN9 */ \
0, /* Channel */ \
},

Configuration data for EzRadio direct rx plug-in.

Definition at line 71 of file ezradio_direct_receive_plugin.h .

Function Documentation

Ecode_t ezradioStartDirectReceive ( EZRADIODRV_Handle_t radioHandle )

Starts direct reception with the radio configurations from the radioHandle parameter.

Parameters
radioHandle Handler of the EzRadio driver instance where channel configuration is set.
Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 54 of file ezradio_direct_receive_plugin.c .

References EZRADIODRV_DirectRxHandle::channel , EZRADIODRV_HandleData::directRx , ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradio_get_int_status() , and ezradio_start_rx() .

Ecode_t ezradioStopDirectReceive ( void )

Stops direct reception.

Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 79 of file ezradio_direct_receive_plugin.c .

References ECODE_EMDRV_EZRADIODRV_OK , and ezradio_change_state() .