IADC_InitSingle_t Struct ReferenceEMLIB > IADC

IADC single init structure

Definition at line 722 of file em_iadc.h .

#include < em_iadc.h >

Data Fields

IADC_Alignment_t alignment
uint8_t dataValidLevel
bool fifoDmaWakeup
bool showId
bool singleTailgate
bool start
IADC_TriggerAction_t triggerAction
IADC_TriggerSel_t triggerSelect

Field Documentation

IADC_Alignment_t IADC_InitSingle_t::alignment

Alignment of data in FIFO.

Definition at line 723 of file em_iadc.h .

Referenced by IADC_initSingle() .

uint8_t IADC_InitSingle_t::dataValidLevel

Data valid level before requesting DMA transfer.

Definition at line 725 of file em_iadc.h .

Referenced by IADC_initSingle() .

bool IADC_InitSingle_t::fifoDmaWakeup

Wake-up DMA when FIFO reaches data valid level.

Definition at line 726 of file em_iadc.h .

Referenced by IADC_initSingle() .

bool IADC_InitSingle_t::showId

Tag FIFO entry with single indicator (0x20).

Definition at line 724 of file em_iadc.h .

Referenced by IADC_initSingle() .

bool IADC_InitSingle_t::singleTailgate

If true, wait until end of SCAN queue before single queue warmup and conversion.

Definition at line 729 of file em_iadc.h .

Referenced by IADC_initSingle() .

bool IADC_InitSingle_t::start

Start scan immediately.

Definition at line 731 of file em_iadc.h .

Referenced by IADC_initSingle() .

IADC_TriggerAction_t IADC_InitSingle_t::triggerAction

Trigger action.

Definition at line 728 of file em_iadc.h .

Referenced by IADC_initSingle() .

IADC_TriggerSel_t IADC_InitSingle_t::triggerSelect

Trigger selection.

Definition at line 727 of file em_iadc.h .

Referenced by IADC_initSingle() .


The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emlib/inc/ em_iadc.h