EEPROMKit Drivers
Detailed Description
I2C EEPROM Driver.
EEPROM I2C driver for 24AA024 (2Kbit) EEPROM device on the EFM32 Development Kits.
Macros |
|
#define | EEPROM_DVK_ADDR 0xA0 |
#define | EEPROM_DVK_LEN 0x100 |
#define | EEPROM_DVK_PAGESIZE 16 |
Functions |
|
static int | EEPROM_AckPoll (I2C_TypeDef *i2c, uint8_t addr) |
Do acknowledge polling on EEPROM device.
|
|
int | EEPROM_Read (I2C_TypeDef *i2c, uint8_t addr, unsigned int offset, uint8_t *data, unsigned int len) |
Read data from EEPROM.
|
|
int | EEPROM_Write (I2C_TypeDef *i2c, uint8_t addr, unsigned int offset, uint8_t *data, unsigned int len) |
Write data to EEPROM.
|
|
Macro Definition Documentation
#define EEPROM_DVK_ADDR 0xA0 |
I2C device address for EEPROM on DK
Definition at line
55
of file
eeprom.h
.
#define EEPROM_DVK_LEN 0x100 |
Number of bytes in EEPROM
Definition at line
57
of file
eeprom.c
.
Referenced by EEPROM_Read() , and EEPROM_Write() .
#define EEPROM_DVK_PAGESIZE 16 |
Function Documentation
|
static |
Do acknowledge polling on EEPROM device.
When writing to an EEPROM, the EEPROM device will be busy for some time after issuing a (page) write. During this time, the EEPROM is not accessible, and will therefore not ACK any requests. This feature can be used to determine when the write is actually completed, and is denoted acknowledgement polling.
- Note
- This function will not return until the EEPROM device acknowledges (or some sort of I2C failure occurs). If trying to acknowledge poll a non-existing device, NACK will always result and this function will never return. Thus, it should not be used unless the EEPROM device is actually present.
- Parameters
-
[in] i2c
Pointer to I2C peripheral register block. [in] addr
I2C address for EEPROM, in 8 bit format, where LSB is reserved for R/W bit.
- Returns
- Returns 0 when EEPROM acknowledges. Negative value is returned is some sort of error occurred during acknowledgement polling.
Definition at line
94
of file
eeprom.c
.
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE , I2CSPM_Transfer() , i2cTransferDone , i2cTransferNack , and I2C_TransferSeq_TypeDef::len .
Referenced by EEPROM_Write() .
int EEPROM_Read | ( | I2C_TypeDef * |
i2c,
|
uint8_t |
addr,
|
||
unsigned int |
offset,
|
||
uint8_t * |
data,
|
||
unsigned int |
len
|
||
) |
Read data from EEPROM.
- Parameters
-
[in] i2c
Pointer to I2C peripheral register block. [in] addr
I2C address for EEPROM, in 8 bit format, where LSB is reserved for R/W bit. [in] offset
Offset in EEPROM to start reading from. [out] data
Location to place read data, must be at least len
long.[in] len
Number of bytes to read.
- Returns
- Returns number of bytes read. Less than specified number of bytes is returned if reading beyond end of EEPROM. Negative value is returned is some sort of error occurred during read.
Definition at line
150
of file
eeprom.c
.
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , EEPROM_DVK_LEN , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE_READ , I2CSPM_Transfer() , i2cTransferDone , and I2C_TransferSeq_TypeDef::len .
int EEPROM_Write | ( | I2C_TypeDef * |
i2c,
|
uint8_t |
addr,
|
||
unsigned int |
offset,
|
||
uint8_t * |
data,
|
||
unsigned int |
len
|
||
) |
Write data to EEPROM.
- Parameters
-
[in] i2c
Pointer to I2C peripheral register block. [in] addr
I2C address for EEPROM, in 8 bit format, where LSB is reserved for R/W bit. [in] offset
Offset in EEPROM to start writing to. [out] data
Location holding data to write, must be at least len
long.[in] len
Number of bytes to write.
- Returns
- Returns number of bytes written. Less than specified number of bytes is returned if writing beyond end of EEPROM. Negative value is returned is some sort of error occurred during write.
Definition at line
211
of file
eeprom.c
.
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , EEPROM_AckPoll() , EEPROM_DVK_LEN , EEPROM_DVK_PAGESIZE , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE_WRITE , I2CSPM_Transfer() , i2cTransferDone , and I2C_TransferSeq_TypeDef::len .