CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU

HFXO initialization structure. Init values should be obtained from a configuration tool, app. note or xtal datasheet.

Definition at line 559 of file em_cmu.h .

#include < em_cmu.h >

Data Fields

uint8_t coreBiasAna
uint8_t coreBiasStartup
CMU_HfxoCoreDegen_TypeDef coreDegenAna
CMU_HfxoCtuneFixCap_TypeDef ctuneFixAna
uint8_t ctuneXiAna
uint8_t ctuneXiStartup
uint8_t ctuneXoAna
uint8_t ctuneXoStartup
bool disOnDemand
bool enXiDcBiasAna
bool forceEn
bool forceXi2GndAna
bool forceXo2GndAna
uint8_t imCoreBiasStartup
CMU_HfxoOscMode_TypeDef mode
bool regLock
CMU_HfxoCbLsbTimeout_TypeDef timeoutCbLsb
CMU_HfxoSteadyStateTimeout_TypeDef timeoutSteady
CMU_HfxoSteadyStateTimeout_TypeDef timeoutSteadyFirstLock

Field Documentation

uint8_t CMU_HFXOInit_TypeDef::coreBiasAna

Core bias current.

Definition at line 571 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::coreBiasStartup

Core bias startup current.

Definition at line 565 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

CMU_HfxoCoreDegen_TypeDef CMU_HFXOInit_TypeDef::coreDegenAna

Core degeneration control.

Definition at line 567 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

CMU_HfxoCtuneFixCap_TypeDef CMU_HFXOInit_TypeDef::ctuneFixAna

Fixed tuning capacitance on XI/XO.

Definition at line 568 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::ctuneXiAna

Tuning capacitance on XI.

Definition at line 570 of file em_cmu.h .

Referenced by BSP_initClocks() , and CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::ctuneXiStartup

XI pin startup tuning capacitance.

Definition at line 564 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::ctuneXoAna

Tuning capacitance on XO.

Definition at line 569 of file em_cmu.h .

Referenced by BSP_initClocks() , and CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::ctuneXoStartup

XO pin startup tuning capacitance.

Definition at line 563 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

bool CMU_HFXOInit_TypeDef::disOnDemand

Disable on-demand requests.

Definition at line 576 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

bool CMU_HFXOInit_TypeDef::enXiDcBiasAna

Enable XI internal DC bias.

Definition at line 572 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

bool CMU_HFXOInit_TypeDef::forceEn

Force oscillator enable.

Definition at line 577 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

bool CMU_HFXOInit_TypeDef::forceXi2GndAna

Force XI pin to ground.

Definition at line 575 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

bool CMU_HFXOInit_TypeDef::forceXo2GndAna

Force XO pin to ground.

Definition at line 574 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::imCoreBiasStartup

Core bias intermediate startup current.

Definition at line 566 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

CMU_HfxoOscMode_TypeDef CMU_HFXOInit_TypeDef::mode

Oscillator mode.

Definition at line 573 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

bool CMU_HFXOInit_TypeDef::regLock

Lock register access.

Definition at line 578 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

CMU_HfxoCbLsbTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutCbLsb

Core bias change timeout.

Definition at line 560 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteady

Steady state timeout duration.

Definition at line 562 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteadyFirstLock

Steady state timeout duration for first lock.

Definition at line 561 of file em_cmu.h .

Referenced by CMU_HFXOInit() .


The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emlib/inc/ em_cmu.h