EUSART_IrDAInit_TypeDef Struct Reference
IrDA Initialization structure.
       Definition at line
       
        259
       
       of file
       
        em_eusart.h
       
       .
      
      
       #include <
       
     
        em_eusart.h
       
       >
      
| Data Fields | |
| EUSART_UartInit_TypeDef | init | 
| General EUSART initialization structure. | |
| bool | irDALowFrequencyEnable | 
| Enable the IrDA low frequency mode. Only Rx operation are enabled. | |
| 
          EUSART_IrDAPulseWidth_Typedef
          | irDAPulseWidth | 
| 
          EUSART_IrDARxFilterEnable_TypeDef
          | irDARxFilterEnable | 
| Set to enable filter on IrDA demodulator. | |
Field Documentation
| 
            EUSART_IrDAPulseWidth_Typedef
           EUSART_IrDAInit_TypeDef::irDAPulseWidth | 
Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.
        Definition at line
        
         271
        
        of file
        
         em_eusart.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/super/platform/emlib/inc/
       em_eusart.h