EUSART_IrDAInit_TypeDef Struct Reference
IrDA Initialization structure.
Definition at line 259
of file em_eusart.h
.
#include <
em_eusart.h
>
Data Fields | |
EUSART_UartInit_TypeDef | init |
General EUSART initialization structure. | |
bool | irDALowFrequencyEnable |
Enable the IrDA low frequency mode. Only Rx operation are enabled. | |
EUSART_IrDAPulseWidth_Typedef | irDAPulseWidth |
EUSART_IrDARxFilterEnable_TypeDef | irDARxFilterEnable |
Set to enable filter on IrDA demodulator. | |
Field Documentation
EUSART_IrDAPulseWidth_Typedef EUSART_IrDAInit_TypeDef::irDAPulseWidth |
Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.
Definition at line 271
of file em_eusart.h
.
The documentation for this struct was generated from the following file:
- C:/repos/super/platform/emlib/inc/
em_eusart.h