You are viewing documentation for version:
The structure represents the prepare write response. 
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_prepare_write_resp_s::dev_addr[RSI_DEV_ADDR_LEN]
remote device address 
handle#
uint8_t rsi_ble_prepare_write_resp_s::handle[2]
attribute handle 
offset#
uint8_t rsi_ble_prepare_write_resp_s::offset[2]
attribute value offset 
length#
uint8_t rsi_ble_prepare_write_resp_s::length
length of attribute value 
att_value#
uint8_t rsi_ble_prepare_write_resp_s::att_value[RSI_DEV_ATT_LEN]
This contains the attribute value. The maximum value is 240, refer to RSI_DEV_ATT_LEN Macro