Describe the attribute default, min, and max values.

This struct is required if the attribute mask specifies that this attribute has a known min and max values.

Public Attribute Documentation#

defaultValue#

sl_zigbee_af_default_attribute_value_t sl_zigbee_af_attribute_min_max_value_t::defaultValue

Default value of the attribute.


Definition at line 133 of file app/framework/include/af-types.h

minValue#

sl_zigbee_af_default_attribute_value_t sl_zigbee_af_attribute_min_max_value_t::minValue

Minimum allowed value.


Definition at line 137 of file app/framework/include/af-types.h

maxValue#

sl_zigbee_af_default_attribute_value_t sl_zigbee_af_attribute_min_max_value_t::maxValue

Maximum allowed value.


Definition at line 141 of file app/framework/include/af-types.h