This is a unique identifier for referencing Zigbee Over-the-air upgrade images. It is used by the OTA plugins when passing around information about an upgrade file.

Public Attributes#

uint16_t

Public Attribute Documentation#

manufacturerId#

uint16_t sl_zigbee_af_ota_image_id_t::manufacturerId

Definition at line 1200 of file app/framework/include/af-types.h

imageTypeId#

uint16_t sl_zigbee_af_ota_image_id_t::imageTypeId

Definition at line 1201 of file app/framework/include/af-types.h

firmwareVersion#

uint32_t sl_zigbee_af_ota_image_id_t::firmwareVersion

Definition at line 1202 of file app/framework/include/af-types.h

deviceSpecificFileEui64#

uint8_t sl_zigbee_af_ota_image_id_t::deviceSpecificFileEui64[EUI64_SIZE]

This is only used for device-specific files. It will be set to all zeroes when the image does not have an upgrade destination field in it. Little endian format.


Definition at line 1210 of file app/framework/include/af-types.h