Use for a link key backup.

Each entry notes the EUI64 of the device it is paired to and the key data. This key may be hashed and not the actual link key currently in use.

Public Attributes#

sl_802154_long_addr_t
sl_zigbee_key_data_t

Public Attribute Documentation#

deviceId#

sl_802154_long_addr_t sl_zigbee_af_link_key_backup_data_t::deviceId

Definition at line 1529 of file app/framework/include/af-types.h

key#

sl_zigbee_key_data_t sl_zigbee_af_link_key_backup_data_t::key

Definition at line 1530 of file app/framework/include/af-types.h