Public Attribute Documentation#

proposedProviderId#

uint32_t sl_zigbee_af_device_management_supplier_t::proposedProviderId

Definition at line 1750 of file app/framework/include/af-types.h

implementationDateTime#

uint32_t sl_zigbee_af_device_management_supplier_t::implementationDateTime

Definition at line 1751 of file app/framework/include/af-types.h

providerChangeControl#

uint32_t sl_zigbee_af_device_management_supplier_t::providerChangeControl

Definition at line 1752 of file app/framework/include/af-types.h

proposedProviderName#

uint8_t sl_zigbee_af_device_management_supplier_t::proposedProviderName[SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH+1]

Definition at line 1753 of file app/framework/include/af-types.h

proposedProviderContactDetails#

uint8_t sl_zigbee_af_device_management_supplier_t::proposedProviderContactDetails[SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH+1]

Definition at line 1754 of file app/framework/include/af-types.h