Public Attribute Documentation#

valid#

bool sl_zigbee_af_plugin_price_client_price_t::valid

Definition at line 1035 of file app/framework/include/af-types.h

active#

bool sl_zigbee_af_plugin_price_client_price_t::active

Definition at line 1036 of file app/framework/include/af-types.h

clientEndpoint#

uint8_t sl_zigbee_af_plugin_price_client_price_t::clientEndpoint

Definition at line 1037 of file app/framework/include/af-types.h

providerId#

uint32_t sl_zigbee_af_plugin_price_client_price_t::providerId

Definition at line 1038 of file app/framework/include/af-types.h

rateLabel#

uint8_t sl_zigbee_af_plugin_price_client_price_t::rateLabel[ZCL_PRICE_CLUSTER_MAXIMUM_RATE_LABEL_LENGTH+1]

Definition at line 1039 of file app/framework/include/af-types.h

issuerEventId#

uint32_t sl_zigbee_af_plugin_price_client_price_t::issuerEventId

Definition at line 1040 of file app/framework/include/af-types.h

currentTime#

uint32_t sl_zigbee_af_plugin_price_client_price_t::currentTime

Definition at line 1041 of file app/framework/include/af-types.h

unitOfMeasure#

uint8_t sl_zigbee_af_plugin_price_client_price_t::unitOfMeasure

Definition at line 1042 of file app/framework/include/af-types.h

currency#

uint16_t sl_zigbee_af_plugin_price_client_price_t::currency

Definition at line 1043 of file app/framework/include/af-types.h

priceTrailingDigitAndPriceTier#

uint8_t sl_zigbee_af_plugin_price_client_price_t::priceTrailingDigitAndPriceTier

Definition at line 1044 of file app/framework/include/af-types.h

numberOfPriceTiersAndRegisterTier#

uint8_t sl_zigbee_af_plugin_price_client_price_t::numberOfPriceTiersAndRegisterTier

Definition at line 1045 of file app/framework/include/af-types.h

startTime#

uint32_t sl_zigbee_af_plugin_price_client_price_t::startTime

Definition at line 1046 of file app/framework/include/af-types.h

endTime#

uint32_t sl_zigbee_af_plugin_price_client_price_t::endTime

Definition at line 1047 of file app/framework/include/af-types.h

durationInMinutes#

uint16_t sl_zigbee_af_plugin_price_client_price_t::durationInMinutes

Definition at line 1048 of file app/framework/include/af-types.h

price#

uint32_t sl_zigbee_af_plugin_price_client_price_t::price

Definition at line 1049 of file app/framework/include/af-types.h

priceRatio#

uint8_t sl_zigbee_af_plugin_price_client_price_t::priceRatio

Definition at line 1050 of file app/framework/include/af-types.h

generationPrice#

uint32_t sl_zigbee_af_plugin_price_client_price_t::generationPrice

Definition at line 1051 of file app/framework/include/af-types.h

generationPriceRatio#

uint8_t sl_zigbee_af_plugin_price_client_price_t::generationPriceRatio

Definition at line 1052 of file app/framework/include/af-types.h

alternateCostDelivered#

uint32_t sl_zigbee_af_plugin_price_client_price_t::alternateCostDelivered

Definition at line 1053 of file app/framework/include/af-types.h

alternateCostUnit#

uint8_t sl_zigbee_af_plugin_price_client_price_t::alternateCostUnit

Definition at line 1054 of file app/framework/include/af-types.h

alternateCostTrailingDigit#

uint8_t sl_zigbee_af_plugin_price_client_price_t::alternateCostTrailingDigit

Definition at line 1055 of file app/framework/include/af-types.h

numberOfBlockThresholds#

uint8_t sl_zigbee_af_plugin_price_client_price_t::numberOfBlockThresholds

Definition at line 1056 of file app/framework/include/af-types.h

priceControl#

uint8_t sl_zigbee_af_plugin_price_client_price_t::priceControl

Definition at line 1057 of file app/framework/include/af-types.h