Interpan header used for sending and receiving interpan messages.
Public Attributes#
sl_802154_long_addr_t
sl_802154_short_addr_t
sl_802154_pan_id_t
sl_zigbee_multicast_id_t
Public Attribute Documentation#
messageType#
sl_zigbee_af_interpan_message_type_t sl_zigbee_af_interpan_header_t::messageType
Definition at line
368
of file app/framework/include/af-types.h
longAddress#
sl_802154_long_addr_t sl_zigbee_af_interpan_header_t::longAddress
MAC addressing, which is the destination for outgoing messages and source for incoming messages, which always has a long address.
Definition at line
375
of file app/framework/include/af-types.h
shortAddress#
sl_802154_short_addr_t sl_zigbee_af_interpan_header_t::shortAddress
Definition at line
376
of file app/framework/include/af-types.h
panId#
sl_802154_pan_id_t sl_zigbee_af_interpan_header_t::panId
Definition at line
377
of file app/framework/include/af-types.h
profileId#
sl_zigbee_af_profile_id_t sl_zigbee_af_interpan_header_t::profileId
APS data
Definition at line
382
of file app/framework/include/af-types.h
clusterId#
sl_zigbee_af_cluster_id_t sl_zigbee_af_interpan_header_t::clusterId
Definition at line
383
of file app/framework/include/af-types.h
groupId#
sl_zigbee_multicast_id_t sl_zigbee_af_interpan_header_t::groupId
The groupId is only used for SL_ZIGBEE_AF_INTERPAN_MULTICAST
Definition at line
388
of file app/framework/include/af-types.h
options#
sl_zigbee_af_interpan_options_t sl_zigbee_af_interpan_header_t::options
Definition at line
389
of file app/framework/include/af-types.h