Contain endpoint information about a device.

Public Attribute Documentation#

eui64#

sl_802154_long_addr_t sl_zigbee_af_device_info_t::eui64

Definition at line 1931 of file app/framework/include/af-types.h

endpoints#

sl_zigbee_af_endpoint_info_struct_t sl_zigbee_af_device_info_t::endpoints[SL_ZIGBEE_AF_MAX_ENDPOINTS_PER_DEVICE]

Definition at line 1932 of file app/framework/include/af-types.h

status#

sl_zigbee_af_device_discovery_status_t sl_zigbee_af_device_info_t::status

Definition at line 1933 of file app/framework/include/af-types.h

discoveryFailures#

uint8_t sl_zigbee_af_device_info_t::discoveryFailures

Definition at line 1934 of file app/framework/include/af-types.h

capabilities#

uint8_t sl_zigbee_af_device_info_t::capabilities

Definition at line 1935 of file app/framework/include/af-types.h

endpointCount#

uint8_t sl_zigbee_af_device_info_t::endpointCount

Definition at line 1936 of file app/framework/include/af-types.h

stackRevision#

uint8_t sl_zigbee_af_device_info_t::stackRevision

Definition at line 1937 of file app/framework/include/af-types.h