Contain the superset of values passed to sl_zigbee_incoming_message_handler.
Public Attributes#
sl_zigbee_incoming_message_type_t
sl_zigbee_aps_frame_t *
uint8_t *
uint16_t
uint16_t
uint8_t
int8_t
uint8_t
uint8_t
uint8_t
Public Attribute Documentation#
type#
sl_zigbee_incoming_message_type_t sl_zigbee_af_incoming_message_t::type
The type of the incoming message.
Definition at line
298
of file app/framework/include/af-types.h
apsFrame#
sl_zigbee_aps_frame_t* sl_zigbee_af_incoming_message_t::apsFrame
APS frame for the incoming message.
Definition at line
302
of file app/framework/include/af-types.h
message#
uint8_t* sl_zigbee_af_incoming_message_t::message
The message copied into a flat buffer.
Definition at line
306
of file app/framework/include/af-types.h
msgLen#
uint16_t sl_zigbee_af_incoming_message_t::msgLen
Length of the incoming message.
Definition at line
310
of file app/framework/include/af-types.h
source#
uint16_t sl_zigbee_af_incoming_message_t::source
Two byte node ID of the sending node.
Definition at line
314
of file app/framework/include/af-types.h
lastHopLqi#
uint8_t sl_zigbee_af_incoming_message_t::lastHopLqi
Link quality from the node that last relayed the message.
Definition at line
319
of file app/framework/include/af-types.h
lastHopRssi#
int8_t sl_zigbee_af_incoming_message_t::lastHopRssi
The energy level (in units of dBm) observed during the reception.
Definition at line
323
of file app/framework/include/af-types.h
bindingTableIndex#
uint8_t sl_zigbee_af_incoming_message_t::bindingTableIndex
The index of a binding that matches the message or 0xFF if there is no matching binding.
Definition at line
328
of file app/framework/include/af-types.h
addressTableIndex#
uint8_t sl_zigbee_af_incoming_message_t::addressTableIndex
The index of the entry in the address table that matches the sender of the message or 0xFF if there is no matching entry.
Definition at line
334
of file app/framework/include/af-types.h
networkIndex#
uint8_t sl_zigbee_af_incoming_message_t::networkIndex
The index of the network on which this message was received.
Definition at line
338
of file app/framework/include/af-types.h