Use for the information retrieved during a response to an Ember Bootloader over-the-air query.

Public Attributes#

uint8_t
uint16_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

hardwareTag#

uint8_t sl_zigbee_af_standalone_bootloader_query_response_data_t::hardwareTag[SL_ZIGBEE_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH]

eui64#

uint8_t sl_zigbee_af_standalone_bootloader_query_response_data_t::eui64[EUI64_SIZE]

mfgId#

uint16_t sl_zigbee_af_standalone_bootloader_query_response_data_t::mfgId

bootloaderVersion#

uint16_t sl_zigbee_af_standalone_bootloader_query_response_data_t::bootloaderVersion

capabilities#

uint8_t sl_zigbee_af_standalone_bootloader_query_response_data_t::capabilities

platform#

uint8_t sl_zigbee_af_standalone_bootloader_query_response_data_t::platform

micro#

uint8_t sl_zigbee_af_standalone_bootloader_query_response_data_t::micro

phy#

uint8_t sl_zigbee_af_standalone_bootloader_query_response_data_t::phy

bootloaderActive#

bool sl_zigbee_af_standalone_bootloader_query_response_data_t::bootloaderActive