Represent Endpoint Information Records used by ZLL Commissioning.

Public Attributes#

sl_802154_short_addr_t
uint8_t
uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

networkAddress#

sl_802154_short_addr_t sl_zigbee_af_plugin_zll_commissioning_endpoint_information_record_t::networkAddress

Definition at line 1187 of file app/framework/include/af-types.h

endpointId#

uint8_t sl_zigbee_af_plugin_zll_commissioning_endpoint_information_record_t::endpointId

Definition at line 1188 of file app/framework/include/af-types.h

profileId#

uint16_t sl_zigbee_af_plugin_zll_commissioning_endpoint_information_record_t::profileId

Definition at line 1189 of file app/framework/include/af-types.h

deviceId#

uint16_t sl_zigbee_af_plugin_zll_commissioning_endpoint_information_record_t::deviceId

Definition at line 1190 of file app/framework/include/af-types.h

version#

uint8_t sl_zigbee_af_plugin_zll_commissioning_endpoint_information_record_t::version

Definition at line 1191 of file app/framework/include/af-types.h