A structure containing data for scheduling a scan.

Public Attributes#

sl_zigbee_network_scan_type_t
uint32_t
uint8_t

Public Attribute Documentation#

scanType#

sl_zigbee_network_scan_type_t sl_zigbee_af_plugin_scan_dispatch_scan_data_t::scanType

The 802.15.4 scan type to be scheduled.


Definition at line 114 of file app/framework/plugin/scan-dispatch/scan-dispatch.h

channelMask#

uint32_t sl_zigbee_af_plugin_scan_dispatch_scan_data_t::channelMask

The channel mask to be scanned.


Definition at line 116 of file app/framework/plugin/scan-dispatch/scan-dispatch.h

duration#

uint8_t sl_zigbee_af_plugin_scan_dispatch_scan_data_t::duration

The duration of the scan period, as an exponent.


Definition at line 118 of file app/framework/plugin/scan-dispatch/scan-dispatch.h

handler#

sl_zigbee_af_plugin_scan_dispatch_scan_results_handler_t sl_zigbee_af_plugin_scan_dispatch_scan_data_t::handler

The handler to be called with the scan results.


Definition at line 120 of file app/framework/plugin/scan-dispatch/scan-dispatch.h