The information regarding scan results.
Public Attribute Documentation#
status#
sl_status_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::status
The status indicating the success or failure of a scan.
This member is only valid when sl_zigbee_af_scan_dispatch_scan_results_are_complete returns true.
63
of file app/framework/plugin/scan-dispatch/scan-dispatch.h
rssi#
int8_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::rssi
The RSSI found during a scan.
This member is only valid when sl_zigbee_af_scan_dispatch_scan_results_are_complete returns false.
70
of file app/framework/plugin/scan-dispatch/scan-dispatch.h
channel#
uint8_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::channel
The channel on which the scan is taking place.
This member is only valid when the results are for an energy scan or sl_zigbee_af_scan_dispatch_scan_results_are_complete returns true and sl_zigbee_af_scan_dispatch_scan_results_are_failure returns false. Note that in active scan results, users can find the channel on which the network was found using the network member of this structure.
80
of file app/framework/plugin/scan-dispatch/scan-dispatch.h
lqi#
uint8_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::lqi
The LQI found during the scan.
This member is only valid when the result are for an active scan.
86
of file app/framework/plugin/scan-dispatch/scan-dispatch.h
network#
sl_zigbee_zigbee_network_t* sl_zigbee_af_plugin_scan_dispatch_scan_results_t::network
The Zigbee network found in the scan.
This member is only valid when the result are for an active scan.
92
of file app/framework/plugin/scan-dispatch/scan-dispatch.h
mask#
uint16_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::mask
A mask containing information about the scan.
95
of file app/framework/plugin/scan-dispatch/scan-dispatch.h