Keep track of incoming and outgoing commands for command discovery.

Public Attributes#

uint16_t
uint8_t
uint8_t

Public Attribute Documentation#

clusterId#

uint16_t sl_zigbee_af_command_metadata_t::clusterId

Definition at line 1626 of file app/framework/include/af-types.h

commandId#

uint8_t sl_zigbee_af_command_metadata_t::commandId

Definition at line 1627 of file app/framework/include/af-types.h

mask#

uint8_t sl_zigbee_af_command_metadata_t::mask

Definition at line 1628 of file app/framework/include/af-types.h