Public Attributes#

uint8_t *
uint16_t

Public Attribute Documentation#

gbzCommands#

uint8_t* sl_zigbee_af_gpf_message_t::gbzCommands

Definition at line 1899 of file app/framework/include/af-types.h

gbzCommandsLength#

uint16_t sl_zigbee_af_gpf_message_t::gbzCommandsLength

Definition at line 1900 of file app/framework/include/af-types.h

gbzCommandsResponse#

uint8_t* sl_zigbee_af_gpf_message_t::gbzCommandsResponse

Definition at line 1901 of file app/framework/include/af-types.h

gbzCommandsResponseLength#

uint16_t sl_zigbee_af_gpf_message_t::gbzCommandsResponseLength

Definition at line 1902 of file app/framework/include/af-types.h

messageCode#

uint16_t sl_zigbee_af_gpf_message_t::messageCode

Definition at line 1903 of file app/framework/include/af-types.h