Store scene table entries in RAM or in tokens, depending on a plugin setting. If endpoint field is SL_ZIGBEE_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID, the entry is unused.

Public Attributes#

uint8_t
uint16_t
uint8_t

Public Attribute Documentation#

endpoint#

uint8_t sl_zigbee_af_scene_table_entry_t::endpoint

Definition at line 1008 of file app/framework/include/af-types.h

groupId#

uint16_t sl_zigbee_af_scene_table_entry_t::groupId

Definition at line 1009 of file app/framework/include/af-types.h

sceneId#

uint8_t sl_zigbee_af_scene_table_entry_t::sceneId

Definition at line 1010 of file app/framework/include/af-types.h

transitionTime#

uint16_t sl_zigbee_af_scene_table_entry_t::transitionTime

Definition at line 1014 of file app/framework/include/af-types.h

transitionTime100ms#

uint8_t sl_zigbee_af_scene_table_entry_t::transitionTime100ms

Definition at line 1015 of file app/framework/include/af-types.h