Zigbee Internet Client/Server Remote Binding struct.
Public Attributes#
sl_802154_long_addr_t
uint8_t
uint8_t
uint16_t
sl_802154_long_addr_t
sl_802154_long_addr_t
Public Attribute Documentation#
targetEUI64#
sl_802154_long_addr_t sl_zigbee_af_remote_binding_struct_t::targetEUI64
Definition at line
1931
of file app/framework/include/af-types.h
sourceEndpoint#
uint8_t sl_zigbee_af_remote_binding_struct_t::sourceEndpoint
Definition at line
1932
of file app/framework/include/af-types.h
destEndpoint#
uint8_t sl_zigbee_af_remote_binding_struct_t::destEndpoint
Definition at line
1933
of file app/framework/include/af-types.h
clusterId#
uint16_t sl_zigbee_af_remote_binding_struct_t::clusterId
Definition at line
1934
of file app/framework/include/af-types.h
destEUI64#
sl_802154_long_addr_t sl_zigbee_af_remote_binding_struct_t::destEUI64
Definition at line
1935
of file app/framework/include/af-types.h
sourceEUI64#
sl_802154_long_addr_t sl_zigbee_af_remote_binding_struct_t::sourceEUI64
Definition at line
1936
of file app/framework/include/af-types.h