Use for all trust center backup data.
The 'keyList' pointer must point to an array and 'maxKeyListLength' must be populated with the maximum number of entries the array can hold.
Functions that modify this data structure will populate 'keyListLength' indicating how many keys were actually written into 'keyList'.
Public Attribute Documentation#
extendedPanId#
sl_802154_long_addr_t sl_zigbee_af_trust_center_backup_data_t::extendedPanId
Definition at line
1593
of file app/framework/include/af-types.h
keyListLength#
uint8_t sl_zigbee_af_trust_center_backup_data_t::keyListLength
Definition at line
1594
of file app/framework/include/af-types.h
maxKeyListLength#
uint8_t sl_zigbee_af_trust_center_backup_data_t::maxKeyListLength
Definition at line
1595
of file app/framework/include/af-types.h
keyList#
sl_zigbee_af_link_key_backup_data_t* sl_zigbee_af_trust_center_backup_data_t::keyList
Definition at line
1596
of file app/framework/include/af-types.h